Skip to main content
Graduate
August 20, 2024
Question

X-NUCLEO-IHM12A1 compatibility with Nucleo-F411RE

  • August 20, 2024
  • 1 reply
  • 865 views

Hi, is the X-NUCLEO-IHM12A1 expansion board compatible with Nucleo-F411RE development board?

    This topic has been closed for replies.

    1 reply

    Super User
    August 20, 2024

    The schematic of the  X-NUCLEO-IHM12A1 expansion board is in the Data Brief:

    https://www.st.com/resource/en/data_brief/x-nucleo-ihm12a1.pdf

    So you can see what pins it uses in the Arduino connector, then check that against the Nucleo-F411RE:

    https://www.st.com/en/evaluation-tools/nucleo-f411re.html

     

    Graduate
    August 20, 2024

    Hi Andrew, thank you for your response.

    I reviewed the pinout as you suggested, and the F411RE is identical to the F401RE, which is compatible according to the STM32 Nucleo expansion boards Motor Control Selection Guide document. However, I'm wondering if there are any other considerations besides pinout that would declare a Nucleo board incompatible with the X-NUCLEO-IHM12A1.

    Super User
    August 20, 2024

    @QuickSilver wrote:

    However, I'm wondering if there are any other considerations besides pinout that would declare a Nucleo board incompatible with the X-NUCLEO-IHM12A1.


    It depends what you mean by, "compatible".

    From a hardware perspective, the pinouts are compatible.

    ST provide ready-to-go software for the F401RE (and a few others), but not for every single possible STM32 variant - including the F411RE.

    So you will have to do a little work in adapting the F401RE (or whatever) software to the F411RE.

    So it's "compatible", but not "ready-to-go"  - it requires a little work from you.

    I would suggest that you get a Nucleo-F401RE, and get the software working first on that. Then you will have a Known-Good reference for your port to the F411RE