Skip to main content
Explorer
November 30, 2023
Solved

X-NUCLEO-OUT01A2 compatible with NUCLEO-G474RE development board

  • November 30, 2023
  • 2 replies
  • 2127 views

Any member could advice us whether we could connect the X-NUCLEO-OUT01A2 expansion board to NUCLEO-G474RE development board.

As data brief explanation is "Compatible with STM32 Nucleo development boards" but the recommendation is mentioned " The expansion board can be connected to either a NUCLEO-F401RE or a NUCLEOG431RB development board ". This make us so confused in selection the hardware.

Thanks.

 

    This topic has been closed for replies.
    Best answer by Pat_ST

    Hello VOANHV, 

    Yes, in fact, the X-NUCLEO-OUT01A2 card is compatible with the NUCLEO-G474RE card, in the same way as it is with the NUCLEO-F401RE or NUCLEO-G431RB cards, because they are in fact Arduino compatible...

    In addition, for information, the both products NUCLEOG431RB and NUCLEO-G474RE are the same, only the MCU is changed.

    Hope this answer to your question.

    With my best regards

    2 replies

    ST Employee
    November 30, 2023

    Hello @VOANHVU 

    According to UM3184, The expansion board can be connected to either a NUCLEO-F401RE or a NUCLEO-G431RB development board.

    Theoretically, the NUCLEO-G474RE and X-NUCLEO-OUT01A2 both follow the Arduino Uno V3 connectivity standard (that's why it says compatible with STM32 Nucleo board), however, there might be incompatibilities with certain features. 

     

    Pat_STAnswer
    ST Employee
    November 30, 2023

    Hello VOANHV, 

    Yes, in fact, the X-NUCLEO-OUT01A2 card is compatible with the NUCLEO-G474RE card, in the same way as it is with the NUCLEO-F401RE or NUCLEO-G431RB cards, because they are in fact Arduino compatible...

    In addition, for information, the both products NUCLEOG431RB and NUCLEO-G474RE are the same, only the MCU is changed.

    Hope this answer to your question.

    With my best regards

    VOANHVUAuthor
    Explorer
    December 4, 2023

    Thank for your support!

    Best regards,