X-NUCLEO-PLM01A1 What is PLM Connector?
Hello,
I'm interested in Power Line Communication and the X-NUCLEO-PLM01A1.
I would like to confirm before purchasing.

What is the role of the PLM connector (CN1)?
Is it a PLC line?
If so, is the Lab DC Supply Inout Connector (CN2) just a power supply?
The PLM Connector appears to be a Power Amplifier Output. Does this Connector use a PLC Line?
To connect two or more boards, you need to connect the PLM Connector (CN1) to each other.
What is the role of CN1?
Will it be a problem if I don't connect the CN1s to each other?
*This post has been translated from Korean to comply with the ST Community guidelines.