Skip to main content
November 21, 2025
Question

2nd Camera for NUCLEO-N657X0-Q

  • November 21, 2025
  • 2 replies
  • 170 views

Hello!
I have NUCLEO-N657X0-Q development kit and two camera modules: B-CAMS-IMX and B-CAMS-OMV.

According to the chip documentation, it is possible to connect two cameras by using CSI-2 as the primary interface and DCMI as the auxiliary interface. However, in the example projects for the N6 series, I only see implementations for working with a single camera connected via CSI-2.

 

1. Is it possible to implement such a dual-camera setup within a single project?
2. Are there any code examples available that demonstrate how to connect both cameras (one via CSI-2 and the other via DCMI)?
3. If no such example exists for dual-camera setups, are there at least examples showing how to connect a single camera via DCMI to an N6-series chip?

 

Any guidance or resources would be greatly appreciated!

2 replies

Technical Moderator
November 21, 2025
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
November 21, 2025

Hello!

Yes, I have seen these examples.
The readme says they are with the OV5640 camera, but I don't see any libraries for it in the project.
I see libraries for the camera sensor IMX335, which is connected via CSI_DCMIPP (not the usual parallel DCMI).

Peter BENSCH
Technical Moderator
December 10, 2025

Thread created by an account from the embargoed country Russian Federation