Skip to main content
Associate III
February 20, 2026
Question

A submodule project in another project

  • February 20, 2026
  • 1 reply
  • 122 views

Hello,

I am working with STM32 IDE v2 and stm32u585 processors. I have a project which is configured with the help of stm32 cube mx and has its own core/Drivers/.ioc files. It is like a ground for using the processor together with other external modules, like sensors, flash chip, LED drivers which are on the same PCB together with the MCU. I have two products using a processor of this family - one is with 64 pins and other with 100 pins. But they have basiccally the same hardware design and use the same pin mapping and peripherals as close as possible to one another. So both can use the same ground project and its configuration and picking different peripherals based on needs. The customer interface is defined separately, in a project that used to be called Application where MMI part is. It is a higher level project and does not need to know what hw there is. Before it was possible to have the ground project as a submodule to  a couple of application projects and it was building with a different IDE and MCU (another producer) 
I have not found still how this option can work with STM32 IDE. If I create an app project in the IDE and add Ground project I get error about not finding a directory although I have added all necessary folders in the Include paths. I want the .ioc / core /drivers to be used drom the ground project and not create a new one. I linked the ground project to the app project but did not help. 
 Is there a way to use another STM32 project as a subproject (or ground) and change only the main project (Application). and in case the subproject changes to easily pull the updated one into several main projects. 
I will appreciate any tips and advice. 

1 reply

Andrew Neil
Super User
February 20, 2026
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.