Skip to main content
carlesls2
Associate III
June 17, 2025
Solved

ADC external channels doubt

  • June 17, 2025
  • 2 replies
  • 354 views

I use the STM32CubeIDE Version: 1.18.1 and the stm32g030k8.

I have a hardware that uses a firmware. This firmware correctly returns the values of the ADC. The ADC is linked to a DMA. 

Channel 4 == 2545 (this is a voltage divisor) 12.5 volts

Channel 10 == 1 (this is connected to a current shunt resistor) No current, then almost 0. 

Channel Temperature == 929

Channel Vreference == 1506

 

 

carlesls2_1-1750147679960.png

 

I develop a new firmware with the very same hardware (not just same design but same device). I apply debug optimization. I use ADC1 with the DMA, first I use the ioc file to set up the ADC and then I copy the MX_ADC1_Initfrom the other stm32cubeide project. 

Yet It does not return the same value from the external pins. Why is that?

 

carlesls2_2-1750148586492.png

 

Thanks for all. 

 

 

 

 

 

Best answer by carlesls2

Solved!

HAL_ADC_Start(&hadc1); and  HAL_ADCEx_Calibration_Start(&hadc1); were missing on the new firmware. 

If the ADC is not callibrated it will return values like 82 and 83 instead of 0.

2 replies

mƎALLEm
Technical Moderator
June 17, 2025

Hello,


@carlesls2 wrote:

I have a hardware that uses a firmware. This firmware correctly returns the values of the ADC.


Firmware that you don't have the code source?

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
carlesls2
carlesls2Author
Associate III
June 17, 2025

I have the code. 

Let me copy it here. 

This is the configuration for the ADC in the former project and it works.

/**
 ******************************************************************************
 * @file $ADC.c
 * @date $12/06/2024
 * @brief
 *
 * @headerfile ${headerfile}
 *
 * @defgroup ${name}
 * @{
 * @ingroup ${name}
 * @{
 * @details
 *
 * @note
 *
 * @see
 *
 * @warning
 *
 * @bug
 *
 ******************************************************************************
 * @attention
 *
 *
 ******************************************************************************
 */

/* Includes ------------------------------------------------------------------*/
#include <HAL/ADC.h>
#include <stdio.h>
/* Private includes ----------------------------------------------------------*/
#include "APP_Config.h"
#include "main.h"


/* Private define ------------------------------------------------------------*/

//------------------------------------------------------------------------------
/* Set Debugger configurations
 * This set, configure debugger systems
 */
#ifdef DEBUG
 //#define DEBUG_RTT_ADC // Enable Segger RTT
#endif


//------------------------------------------------------------------------------
/* Set ADC conversions
 * This set, configure ADC module
 */
#define ADC_CHANEL_NUMBER 4 //!< [uint8_t] number of channels ADC
#define ADC_SAMPLES 4 //!< [uint8_t] number of samples for the mean

#define DIGITAL_SCALE_12BITS ((uint32_t) 0xFFF) // Full-scale digital value with a resolution of 12 bits
#define VAR_CONVERTED_DATA_INIT_VALUE (DIGITAL_SCALE_12BITS + 1) // Init variable out of ADC expected conversion data range
#define ADC_CONVERTED_DATA_BUFFER_SIZE ((uint32_t) 4) // Definition of ADCx conversions data table size
#define VDDA_APPLI (3300U) // [mV] Value of analog reference voltage (Vref+), connected to analog voltage

#define CHANNEL_VBAT 0 // Array Position
#define CHANNEL_CURRENT 1
#define CHANNEL_TEMPERATURE 2
#define CHANNEL_VREF 3

#define ADC_VBAT_OFFSET +000 //!< [uint8_t] [mV] Correction factor of voltage battery
 #define ADC_VBAT_R1 10000 //!< [uint16_t] Div R1 resistor value
 #define ADC_VBAT_R2 2200 //!< [uint16_t] Div R2 Shunt resistor value

#define ADC_MOTOR_SHUNT_OFFSET +0.0f //!< [uint8_t] Correction factor of current shunt voltage
#define ADC_SHUNT 0.01f //!< [uint8_t] Shunt resistor value


/* Private typedef -----------------------------------------------------------*/
ADC_HandleTypeDef hadc1;


/* Private macro -------------------------------------------------------------*/



/* Private variables ---------------------------------------------------------*/
/**
 * @brief Array where the new value will be added.
 */
volatile uint16_t ADC_DMA_Buff[4];
volatile uint32_t ADC_Average_Buff[ADC_CHANEL_NUMBER];
volatile uint8_t ADC_Samples = 0;

volatile uint16_t VoltageReference_Dig =0; // [uint16_t] [ADC] Average sum for digital value
volatile uint16_t VoltageBattery_Dig =0; // [uint16_t] [ADC]
volatile uint16_t VoltageMotorShunt_Dig =0; // [uint16_t] [ADC]
volatile int16_t Temperature_Dig =0; // [ int16_t] [ADC]

volatile uint16_t VoltageBattery_Pin =0; // [ int16_t] [mV] Pin Voltage input to ADC
volatile uint16_t VoltageMotorShunt_Pin =0; // [ int16_t] [mV] Pin Voltage input to ADC

volatile uint16_t VoltageReference =0; //!< [uint16_t] [mV] ADC Voltage Reference Average
volatile int16_t VoltageBattery = 0; //!< [int16_t] [mV] Voltage Battery Average
volatile int16_t CurrentMotor =0; //!< [int16_t] [mA] Voltage Motor Shunt Average
volatile int16_t Temperature =0; //!< [ int16_t] [0.01ºC] Tj microcontroller Average temperature, ±º2C aucrany

volatile uint16_t VoltageBatteryVirtual =0; //!< [uint16_t] [mV] Voltage Battery Average
volatile int16_t CurrentMotorVirtual =0; //!< [uint16_t] [mA] Voltage Motor Shunt Average
volatile int16_t TemperatureVirtual =0; //!< [ int16_t] [0.01ºC] Tj microcontroller Average temperature, ±º2C aucrany

volatile float ConversionFloat_Auxiliar=0.0f;
/* Private function prototypes -----------------------------------------------*/



/* Private user code ---------------------------------------------------------*/



/**
 * @brief This function's role is to initialise the 4 ADC's value
 * which are:
 * [CHANEL_VREF]
 * [CHANEL_VBAT]
 * [CHANEL_CURRENT]
 * [CHANEL_TEMPERATURE]
 *
 */
void HAL_ADC_Init_vars(void)
{
	//--------------------------
	for (uint8_t idx = 0; idx < ADC_CHANEL_NUMBER; idx++)
	{
		ADC_DMA_Buff[idx] = 0;
		ADC_Average_Buff[idx] = 0;
	}
	ADC_Samples = 0;
	VoltageReference_Dig = 0;
	VoltageBattery_Dig = 0;
	VoltageMotorShunt_Dig = 0;
	Temperature_Dig = 0;
	VoltageBattery_Pin = 0;
	VoltageReference = 0;
	VoltageBattery = 0;
	CurrentMotor = 0.0;
	Temperature = 0;
	 ConversionFloat_Auxiliar=0.0f;
	//--------------------------
}// End HAL_ADC_Init_vars



/**
 * @brief This is an interruption that occurs whenever the DMA is ready to deliver a new ADC value/sample
 *
 */
 void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc1)
{


	ADC_Average_Buff[CHANNEL_VREF] = ADC_DMA_Buff[CHANNEL_VREF];
	ADC_Average_Buff[CHANNEL_VBAT] = ADC_DMA_Buff[CHANNEL_VBAT];
	ADC_Average_Buff[CHANNEL_CURRENT] = ADC_DMA_Buff[CHANNEL_CURRENT];
	ADC_Average_Buff[CHANNEL_TEMPERATURE] = ADC_DMA_Buff[CHANNEL_TEMPERATURE];
	ADC_Average_Buff[CHANNEL_VREF] += ADC_DMA_Buff[CHANNEL_VREF];
	ADC_Average_Buff[CHANNEL_VBAT] += ADC_DMA_Buff[CHANNEL_VBAT];
	ADC_Average_Buff[CHANNEL_CURRENT] += ADC_DMA_Buff[CHANNEL_CURRENT];
	ADC_Average_Buff[CHANNEL_TEMPERATURE] += ADC_DMA_Buff[CHANNEL_TEMPERATURE];
	//-------------------------------------------------------------
	if (ADC_Samples >= ADC_SAMPLES - 1)
	{
		//------------------------------
		// Voltage Reference calculation
		if (ADC_Average_Buff[CHANNEL_VREF] > 0)
		{
			VoltageReference_Dig = (uint16_t) ADC_Average_Buff[CHANNEL_VREF]	/ ADC_SAMPLES;
			VoltageReference = (uint16_t) __LL_ADC_CALC_VREFANALOG_VOLTAGE(	VoltageReference_Dig, LL_ADC_RESOLUTION_12B);
		}
		else
		{
			VoltageReference = VDDA_APPLI;
			// WARNING: Measure error, action: pending.
		}
		//------------------------------
		// Voltage Battery calculation
		if (ADC_Average_Buff[CHANNEL_VBAT] > 0)
		{
			VoltageBattery_Dig = (uint16_t) ADC_Average_Buff[CHANNEL_VBAT]/ ADC_SAMPLES;
			VoltageBattery_Pin = (uint16_t) __LL_ADC_CALC_DATA_TO_VOLTAGE(	VoltageReference, VoltageBattery_Dig,LL_ADC_RESOLUTION_12B);
			ConversionFloat_Auxiliar = (float) (VoltageBattery_Pin);
			if (ConversionFloat_Auxiliar > 0)
			{
				ConversionFloat_Auxiliar = ((((ConversionFloat_Auxiliar / 1000)	/ ADC_VBAT_R2) * (ADC_VBAT_R2 + ADC_VBAT_R1)) * 1000)+ ADC_VBAT_OFFSET;
				//ConversionFloat_Auxiliar /= 1000;
			}
			else
			{
				ConversionFloat_Auxiliar = 0;
			}
			VoltageBattery = (uint16_t)ConversionFloat_Auxiliar;
		}
		else
		{
			// WARNING: Measure error, action: pending.
		}
		//------------------------------
		// Current Motor calculation
		if (ADC_Average_Buff[CHANNEL_CURRENT] > 0) // index == 1
		{
			VoltageMotorShunt_Dig = (uint16_t) ADC_Average_Buff[CHANNEL_CURRENT]	/ ADC_SAMPLES;
			VoltageMotorShunt_Pin = (uint16_t) __LL_ADC_CALC_DATA_TO_VOLTAGE(	VoltageReference, VoltageMotorShunt_Dig,
					LL_ADC_RESOLUTION_12B);
			ConversionFloat_Auxiliar = (float) (VoltageMotorShunt_Pin);
			if (ConversionFloat_Auxiliar > 0)
			{
				ConversionFloat_Auxiliar = (((ConversionFloat_Auxiliar / 1000)/ ADC_SHUNT) * 1000) + ADC_MOTOR_SHUNT_OFFSET;
			}
			else
			{
				ConversionFloat_Auxiliar = 0;
			}
			CurrentMotor = ConversionFloat_Auxiliar;
		}
		else
		{
			// WARNING: Measure error, action: pending.
		}
		//------------------------------
		// Temperature calculation
		if (ADC_Average_Buff[CHANNEL_TEMPERATURE] > 0)
		{
			Temperature_Dig = (uint16_t) ADC_Average_Buff[CHANNEL_TEMPERATURE]	/ ADC_SAMPLES;
			Temperature = 100*(int16_t) __LL_ADC_CALC_TEMPERATURE(VoltageReference,	Temperature_Dig, LL_ADC_RESOLUTION_12B);
		}
		else
		{
			// WARNING: Measure error, action: pending.
		}
		//------------------------------
		// Initialization buffers
		ADC_Samples = 0;
		ADC_Average_Buff[CHANNEL_VREF] = 0;
		ADC_Average_Buff[CHANNEL_VBAT] = 0;
		ADC_Average_Buff[CHANNEL_CURRENT] = 0;
		ADC_Average_Buff[CHANNEL_TEMPERATURE] = 0;
		//------------------------------

		//------------------------------
	}
	else
	{
		ADC_Samples++;
	}
} // End HAL_ADC_ConvCpltCallback



/* Public user code ---------------------------------------------------------*/



//------------------------------------------------------------------------------
/**
 * @brief Return Voltage Battery.
 * @PAram None
 * @retval [uint16_t] [mV] Voltage Battery
 */
uint16_t ADC_Voltage_Battery_Get(void){

 return VoltageBattery;

}// End Voltage_Battery_Get


//------------------------------------------------------------------------------
/**
 * @brief Set Voltage Battery Virtual
 * @PAram Value
*/
void HAL_ADC_Voltage_Battery_Virtual_Set(uint16_t Value){
 VoltageBatteryVirtual=Value;
}// End HAL_ADC_Voltage_Battery_Virtual_Set



//------------------------------------------------------------------------------
/**
 * @brief Return Current Motor.
 * @PAram None
 * @retval [uint16_t] [mA] Motor Current
 */
int16_t HAL_ADC_Current_Motor_Get(void){

 return CurrentMotor;

}// End HAL_ADC_Current_Motor_Get


//------------------------------------------------------------------------------
/**
 * @brief Set Current Motor Virtual
 * @PAram Value
*/
void HAL_ADC_Current_Motor_Virtual_Set(int16_t Value){
 CurrentMotorVirtual=Value;
}// End HAL_ADC_Current_Motor_Virtual_Set



//------------------------------------------------------------------------------
/**
 * @brief Return Temperature Average.
 * @PAram None
 * @retval [ int16_t] [0.01ºC] Microcontroller temperature
 */
int16_t HAL_ADC_Temperature_Get(void){
 return Temperature;
}// End HAL_ADC_Temperature_Get


//------------------------------------------------------------------------------
/**
 * @brief Set Temperature Virtual
 * @PAram Value
*/
void HAL_ADC_Temperature_Virtual_Set(int16_t Value){
 TemperatureVirtual=Value;
}// End HAL_ADC_Temperature_Virtual_Set



/**
 * @brief This function's role is to connect the ADC to the DMA and to indicate the dedicated buffer to do it.
 *
 */
void MX_ADC1_Start(void){
 HAL_ADCEx_Calibration_Start(&hadc1);
 HAL_ADC_Start_DMA(&hadc1,(uint32_t *)ADC_DMA_Buff, ADC_CHANEL_NUMBER);
 HAL_ADC_Start(&hadc1);
}// End MX_ADC1_Start


/**
 * @brief This function's role is to initialise the ADC peripheral and how it should behave.
 */
void MX_ADC1_Init(void) {
 ADC_ChannelConfTypeDef sConfig = {0};
 //------------------------------------------------------
 //------------------------------------------------------
 //Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV128;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.LowPowerAutoPowerOff = DISABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.NbrOfConversion = 4;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_160CYCLES_5;
 hadc1.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_160CYCLES_5;
 hadc1.Init.OversamplingMode = DISABLE;
 hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
 if (HAL_ADC_Init(&hadc1) != HAL_OK){
 Error_Handler();
 }
 // Configure Regular Channel
 sConfig.Channel = ADC_CHANNEL_4;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK){
 Error_Handler();
 }
 //Configure Regular Channel
 sConfig.Channel = ADC_CHANNEL_10;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {
 Error_Handler();
 }
 // Configure Regular Channel
 sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
 sConfig.Rank = ADC_REGULAR_RANK_3;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK){
 Error_Handler();
 }
 // Configure Regular Channel
 sConfig.Channel = ADC_CHANNEL_VREFINT;
 sConfig.Rank = ADC_REGULAR_RANK_4;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK){
 Error_Handler();
 }
 //------------------------------------------------------


}//End MX_ADC1_Init

 

And this is the new project that is unable to write or produce a valid ADC value.

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */


/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

UART_HandleTypeDef huart2;
DMA_HandleTypeDef hdma_usart2_rx;
DMA_HandleTypeDef hdma_usart2_tx;

/* USER CODE BEGIN PV */
#define ADC_BUF_SIZE		(uint8_t)4
#define TX_BUF_SIZE 		(uint8_t)64
#define RX_BUF_SIZE 		(uint8_t)64

volatile uint8_t uart_tx_buffer[TX_BUF_SIZE];
volatile uint8_t uart_rx_buffer[RX_BUF_SIZE];
volatile uint16_t adc_data_buffer[ADC_BUF_SIZE];


/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_ADC1_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */


void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart) {
 if (huart->Instance == USART2) {
 // Tx complete, optionally signal application task
 }
}

void HAL_UART_RxHalfCpltCallback(UART_HandleTypeDef *huart) {
 if (huart->Instance == USART2) {
 // Process first half of uart_rx_buffer
 }
}

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) {
 if (huart->Instance == USART2) {
 // Process second half of uart_rx_buffer
 	for(uint8_t c_i = 0 ; c_i < TX_BUF_SIZE; c_i++)
 	{
 		uart_tx_buffer[c_i] = '\0';
 	}
 	uart_tx_buffer[0] = 'c';
 	uart_tx_buffer[1] = 'a';
 	uart_tx_buffer[2] = 'c';
 	uart_tx_buffer[3] = 'a';
 	HAL_UART_Transmit_DMA(&huart2, uart_tx_buffer, 5);
 }
}

void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc) {
 if (hadc->Instance == ADC1) {
 // Process first half of adc_data_buffer
 }
}

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) {
 if (hadc->Instance == ADC1) {
 // Process second half of adc_data_buffer
 }
}




/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 MX_USART2_UART_Init();
 /* USER CODE BEGIN 2 */


 // Start UART RX DMA in circular mode
 HAL_UART_Receive_DMA(&huart2, uart_rx_buffer, RX_BUF_SIZE);

 // Start ADC DMA in circular mode
 HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc_data_buffer, ADC_BUF_SIZE);
 // If ADC is triggered by a timer:
 // HAL_TIM_Base_Start(&htimx); // Or HAL_TIM_PWM_Start() if using PWM trigger

 // For UART TX, you'll trigger it as needed:
 // HAL_UART_Transmit_DMA(&huartx, uart_tx_buffer, tx_length);



 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV64;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.LowPowerAutoPowerOff = DISABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.NbrOfConversion = 4;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_160CYCLES_5;
 hadc1.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_160CYCLES_5;
 hadc1.Init.OversamplingMode = DISABLE;
 hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_4;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_10;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
 sConfig.Rank = ADC_REGULAR_RANK_3;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_VREFINT;
 sConfig.Rank = ADC_REGULAR_RANK_4;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 // Configure Regular Channel
//	sConfig.Channel = ADC_CHANNEL_4;
//	sConfig.Rank = ADC_REGULAR_RANK_1;
//	sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
//	if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {
//		Error_Handler();
//	}
//	//Configure Regular Channel
//	sConfig.Channel = ADC_CHANNEL_10;
//	sConfig.Rank = ADC_REGULAR_RANK_2;
//	if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {
//		Error_Handler();
//	}
//	// Configure Regular Channel
//	sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
//	sConfig.Rank = ADC_REGULAR_RANK_3;
//	if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {
//		Error_Handler();
//	}
//	// Configure Regular Channel
//	sConfig.Channel = ADC_CHANNEL_VREFINT;
//	sConfig.Rank = ADC_REGULAR_RANK_4;
//	if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {
//		Error_Handler();
//	}



 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief USART2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{

 /* USER CODE BEGIN USART2_Init 0 */

 /* USER CODE END USART2_Init 0 */

 /* USER CODE BEGIN USART2_Init 1 */

 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */

 /* USER CODE END USART2_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
 /* DMA1_Channel2_3_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel2_3_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

carlesls2
carlesls2AuthorBest answer
Associate III
June 17, 2025

Solved!

HAL_ADC_Start(&hadc1); and  HAL_ADCEx_Calibration_Start(&hadc1); were missing on the new firmware. 

If the ADC is not callibrated it will return values like 82 and 83 instead of 0.