Skip to main content
Associate III
November 6, 2025
Question

ADC not started by TIM output trigger

  • November 6, 2025
  • 4 replies
  • 284 views

I'm using the STM32H562. I'm trying to start an ADC conversion using output compare on a specified channel during the middle of an up-down count of a timer.

Timer used: TIM8 running at 250 MHz, generating a 20 kHz period
Channel: 4
Timing: At the peak of the up-down count

Peripheral configuration:

  • In TIM8_CCMR2, OC3M is set to 0001 to activate the signal when the counter matches the compare value.
  • In TIM8_CR2, both MMS and MMS2 are set to 0111 to use Channel 4 as the trigger output.
  • For ADC1 and ADC2, the trigger source is set to TIM8 TRG2.

Although TIM8 has been started, the HAL status of the ADC conversion remains at 0xFF.
I would like to know if there is any configuration I might have overlooked, or if there is a way to detect the start of ADC conversion for debugging purposes, such as using an interrupt.

 

Here are the initialization procedures for TIM and ADC:

/**
 * @brief TIM8 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM8_Init(void)
{

 /* USER CODE BEGIN TIM8_Init 0 */

 /* USER CODE END TIM8_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};

 /* USER CODE BEGIN TIM8_Init 1 */

 /* USER CODE END TIM8_Init 1 */
 htim8.Instance = TIM8;
 htim8.Init.Prescaler = 0;
 htim8.Init.CounterMode = TIM_COUNTERMODE_CENTERALIGNED1;
 htim8.Init.Period = 6249;
 htim8.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim8.Init.RepetitionCounter = 0;
 htim8.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 if (HAL_TIM_Base_Init(&htim8) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim8, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_Init(&htim8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_OC_Init(&htim8) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC4REF;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_OC4REF;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim8, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM2;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_ACTIVE;
 sConfigOC.Pulse = 3125;
 if (HAL_TIM_OC_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_4) != HAL_OK)
 {
 Error_Handler();
 }
 __HAL_TIM_ENABLE_OCxPRELOAD(&htim8, TIM_CHANNEL_4);
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.BreakFilter = 0;
 sBreakDeadTimeConfig.BreakAFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
 sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
 sBreakDeadTimeConfig.Break2Filter = 0;
 sBreakDeadTimeConfig.Break2AFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim8, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM8_Init 2 */
 __HAL_TIM_SET_COMPARE(&htim8, TIM_CHANNEL_4, 6249/2);

 /* USER CODE END TIM8_Init 2 */
 HAL_TIM_MspPostInit(&htim8);

}

 

/**
 * @brief ADC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.NbrOfConversion = 2;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T8_TRGO2;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief ADC2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC2_Init(void)
{

 /* USER CODE BEGIN ADC2_Init 0 */

 /* USER CODE END ADC2_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC2_Init 1 */

 /* USER CODE END ADC2_Init 1 */

 /** Common config
 */
 hadc2.Instance = ADC2;
 hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc2.Init.Resolution = ADC_RESOLUTION_12B;
 hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc2.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc2.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc2.Init.LowPowerAutoWait = DISABLE;
 hadc2.Init.ContinuousConvMode = ENABLE;
 hadc2.Init.NbrOfConversion = 2;
 hadc2.Init.DiscontinuousConvMode = DISABLE;
 hadc2.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T8_TRGO2;
 hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc2.Init.DMAContinuousRequests = DISABLE;
 hadc2.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL;
 hadc2.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc2.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_4;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC2_Init 2 */

 /* USER CODE END ADC2_Init 2 */

}

 

4 replies

waclawek.jan
Super User
November 6, 2025

Read out and check/post content of TIM and ADC registers at the moment when you are sure it is supposed to work.

JW

TDK
Super User
November 6, 2025

I don't see you starting the ADC conversion anywhere in the posted code (HAL_ADC_Start_DMA). Just initialization. The timer may trigger it, but you need to start it first.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ThoufielAuthor
Associate III
November 7, 2025

Sorry for the missing description.

In the subsequent process, we are calling HAL_ADC_Start_IT followed by starting TIM8 in that order.

 

By the way, if the ADC is configured for single conversion mode, do we need to call ADC_Start every time a conversion is completed?

Technical Moderator
November 6, 2025
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
ST Employee
November 14, 2025

Hello @Thoufiel ,

Thank you for sharing your configuration details. To help you resolve the TIMx-triggered ADC conversion issue, you can also consider the following steps and clarifications:

1. Set ADC Continuous Conversion Mode to DISABLE
When using an external trigger from a timer (like TIM8 TRGO2), it is recommended to disable continuous conversion mode (ContinuousConvMode = DISABLE). This allows the ADC to start a new conversion sequence only when triggered by the timer event.

2. Configure ADC External Trigger Correctly
Using ADC_EXTERNALTRIG_T8_TRGO2 with rising edge is correct if TIM8 is properly configured to generate TRGO2 on the intended event (such as OC4REF). Confirm that TIM8’s master output trigger 2 is set to TIM_TRGO2_OC4REF and verify its functionality, either via interrupt monitoring or by measuring the signal with an oscilloscope.

3. Verify GPIO Pins Configuration
Make sure ADC input pins are configured in analog mode with no pull-up or pull-down resistors.

4. Start TIM8 Timer and Output Compare Channel Before Starting ADC
Ensure you start the timer base and the OC channel that generates the trigger event before starting ADC conversions:

HAL_TIM_Base_Start(&htim8);
HAL_TIM_OC_Start(&htim8, TIM_CHANNEL_4);

5. Start ADC with Interrupt or Polling Mode
After timer and OC channel are running, start the ADC in interrupt mode with:

HAL_ADC_Start_IT(&hadc1);
HAL_ADC_Start_IT(&hadc2);

 

6.Consider Increasing ADC Sampling Time
Consider increasing the sampling time from 2.5 cycles to at least 7.5 or more, especially if your input signals have higher source impedance. This improves conversion accuracy.

Regarding your question about HAL_ADC_Start_IT in single conversion mode:

  •  the ADC is configured for single conversion mode (ContinuousConvMode = DISABLE and NbrOfConversion = 1), you must call HAL_ADC_Start() or HAL_ADC_Start_IT() each time you want to initiate a new conversion after the previous one completes, since the ADC stops after every conversion.

  • In contrast, when using external trigger mode with multiple conversions in scan mode and continuous mode disabled, the ADC starts a full conversion sequence automatically on each external trigger event. In this case, calling HAL_ADC_Start_IT() once is sufficient to enable the ADC; subsequent conversions are triggered by the timer.

Feel free to share your updated code or any error messages if you need further assistance.

Best regards,

DHIF Khaled

"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"