ADC sampling frequency questions
Doing the set up in MX
I have four ADC channels on APB2 with PCLK2 at 84 MHz sampling 4 microphones.
The recommended audio sampling rate stretch from 44.1 kHz up to 96 kHz, so initially I'm happy anywhere in that range for now.
I have set the clock pre-scaler to divide PCLK2 / 4 so the ADC clock is at 21 MHz
I have 12 bit resolution which takes 15 ADC cycles but then in the "rank" section of the parameter settings there is a pull down for sampling time for each channel. I'm guessing that the value I pass in the "rank" section is what I would use to get the final sampling rate.
e.g. if I chose 84 cycles for each channel then I would have a sample rate of 250 kHz per channel giving a sample rate for all conversions of 62.5 kHz?
Or do I add the sample time to the resolution time e.g. 84+15 giving a sample rate of ~212 kHz per channel?