Skip to main content
Best answer by Bubbles

Hi @jishnu1234 ,

with the H5 series the primary focus is the Secure Manager (closed, secure and certified implementation of ARM PSA), other projects like mbed crypto are also fully supported. What I meant in my previous answer was that if the external entity governing some SW package ceases it's development, it's out of our hands.

ThreadX is also well supported by the H5 as far as I know.

BR,

J

3 replies

Pavel A.
Super User
September 25, 2024

Microsoft won't support Azure RTOS going forward. ST will support Eclipse ThreadX.

Associate II
September 25, 2024

Hi thanks for the reply but this reply from ST employee sounded different to me

jishnu1234_0-1727271901142.png

@Bubbleswould you mind adding some information you have?
The thing is I'm looking for hardware support for TLS crypto in STM32H573 series and wondering how this will be going forward. Will ThreadX have it or are there any other options.

Thanks

Bubbles
BubblesBest answer
ST Employee
September 26, 2024

Hi @jishnu1234 ,

with the H5 series the primary focus is the Secure Manager (closed, secure and certified implementation of ARM PSA), other projects like mbed crypto are also fully supported. What I meant in my previous answer was that if the external entity governing some SW package ceases it's development, it's out of our hands.

ThreadX is also well supported by the H5 as far as I know.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
September 22, 2025

Hey

Sorry to post on an older thread. Does anyone know if the H573 hardware Security features are supported in Zephyr?

I'm trying to enable it / confirm it does but there is very little resource of discussion regarding the H5 and its hardware encryption features.

Cheers

Dave