Skip to main content
Associate III
December 11, 2025
Solved

BSP symbols not recognised by IDE

  • December 11, 2025
  • 1 reply
  • 1215 views

Split from STM32G431CBU: section `.bss' will not fit in region `RAM' as that issue is solved, and this is a new question.


One more question. If you can help.

BSP_TS_Init e BSP_TS_GetState is not recognized in IDE versions 1.19 and 1.20.

Therefore, TOUCH doesn't work.

BSP_TS_Init(ILI9488_TFTHEIGHT, ILI9488_TFTWIDTH);

BSP_TS_GetState(& osc->touchScreen);

What did I forget to port?

Best answer by ValterMatos

I managed to solve it. OK now.
I was having problems with the "stm32_adafruit_ts.c" file.
Code successfully ported to the G431. Only a slight flickering on the display due to low memory.

I didn't give up until I succeeded.
Thank you.

1 reply

Andrew Neil
Super User
December 11, 2025

What do you mean by, "not recognised" ?

Is this just within the Editor, or an actual build error?

 

Does your project contain definitions for those functions?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ValterMatosAuthorBest answer
Associate III
December 11, 2025

I managed to solve it. OK now.
I was having problems with the "stm32_adafruit_ts.c" file.
Code successfully ported to the G431. Only a slight flickering on the display due to low memory.

I didn't give up until I succeeded.
Thank you.