Skip to main content
Associate III
January 29, 2026
Solved

Can I launch a call to SPI with DMA from a timer interrupt?

  • January 29, 2026
  • 1 reply
  • 207 views

I want to make a pedometer app that would count steps and display the number of steps on an LCD screen. 

I have tested my functions for the screen (ILI9341 SPI), and they work successfully. I tested the LCD code by initializing a timer that incremented the value to display every second and sets the flag update_lcd_flag.

But when I add the pedometer code, which uses SPI1, the value on the screen never gets updated past zero. Is it because I launch a DMA interrupt from the timer interrupt, or do I need to look for problems somehwere else, e.g. in my pedometer logic or SPI1 configuration? The pedometer relies on the accelometer, which is built into STM32F4O7G-DISC1, which is my board, by default

P.S. The LCD functions don't use interrupts or DMA, they only use polling.

The timer callback

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef* htim)
{
	 if (htim->Instance == TIM2) {
		 if (draw_ready == 1) {
			 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_RESET);
			 HAL_SPI_TransmitReceive_DMA(&hspi1, xyz_addr, xyz_data, 6);
			 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_SET);
		 }
	 }
	 //else if (htim->Instance == TIM3) {
	 //	 if (draw_ready == 1) {
			 //steps_count += 1;
			 //update_lcd_flag = 1;
	 //	 }
	 //}
}

 The SPI RxTx interrupt

//spi callback function
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef * hspi)
{
	if(hspi == &hspi1) {
		//declare variables
		int16_t x, y, z;
		uint32_t mag;
		uint32_t prev_index, prev_prev_index, prev_sample, prev_prev_sample;
		prev_index = 0; prev_prev_index = 0; prev_sample = 0; prev_prev_sample = 0;
		//calculate magnitude
		x = (int16_t)((int16_t)xyz_data[0] | ((int16_t)xyz_data[1] << 8));
		y = (int16_t)((int16_t)xyz_data[2] | ((int16_t)xyz_data[3] << 8));
		z = (int16_t)((int16_t)xyz_data[4] | ((int16_t)xyz_data[5] << 8));
		mag = (x*x + y*y + z*z); //auto-convert float to int //was sqrt
			last_peak += 1; //when the last time there was a peak
			value_period = 0;
			prev_index = buf_index; //previous sample index
			prev_prev_index = (prev_index == 0) ? (ACC_BUF_SIZE - 1) : (prev_index - 1); //(prev_index - 1) % ACC_BUF_SIZE; //pre-previous sample index
			prev_sample = acc_values_buf[prev_index];
			prev_prev_sample = acc_values_buf[prev_prev_index];
			buf_index = (buf_index + 1) % ACC_BUF_SIZE; //update buf_index
			acc_values_buf[buf_index] = mag; //add the sample
			//make all checks
			if ((last_peak < MAX_PEAK_DIFF && last_peak > MIN_PEAK_DIFF)
				&& (prev_sample > prev_prev_sample
					&& prev_sample > mag)
				&& (prev_sample > PEAK_CUTOFF)) {
					steps_count += 1; //uncomment later
					update_lcd_flag = 1;
					last_peak = 0;
			}
			else {
				//update_lcd_flag = 0;
			}
		//call to SPI again //deprecated
		//HAL_SPI_TransmitReceive_DMA(&hspi1, xyz_addr, xyz_data, 6);
	}
}

 The main function

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */


 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_I2S3_Init();
 MX_SPI1_Init();
 MX_USB_HOST_Init();
 MX_SPI2_Init();
 MX_TIM2_Init();
 MX_TIM3_Init();
 /* USER CODE BEGIN 2 */
 //timers
 HAL_TIM_Base_Start_IT(&htim2);
 HAL_TIM_Base_Start_IT(&htim3);
 //Reset the screen
 ILI9341_Init(&hspi2);
 //screen experiment, delete later (black rectangle)
 HAL_Delay(1000);

 //Write_Rectangle(0, 50, 0, 50, 0, &hspi2); //good
 //draw_digit(10, 10, 12, 8, 0, &hspi2); //good
 //draw_number(UINT32_MAX, 12, &hspi2); //good

 //Set everything for the accelometer
 uint8_t OUT_X_L = 0x28;
 uint8_t OUT_X_H = 0x29;
 uint8_t OUT_Y_L = 0x2A;
 uint8_t OUT_Y_H = 0x2B;
 uint8_t OUT_Z_L = 0x2C;
 uint8_t OUT_Z_H = 0x2D;
 uint8_t CTRL_REG5 = 0x24; //for sensitivity (change from default 2 to 4/8) (bits 5-4)
 //receivers and transmitters
 xyz_addr[0] = OUT_X_L; xyz_addr[1] = OUT_X_H; xyz_addr[2] = OUT_Y_L; xyz_addr[3] = OUT_Y_H; xyz_addr[4] = OUT_Z_L; xyz_addr[5] = OUT_Z_H;
 uint8_t ctrl_val;

 //fill buffer with 0s
 for (int i = 0; i < ACC_BUF_SIZE; i++) {
	 acc_values_buf[i] = 0;
 }
 //receive and set accelerator sensitivity
 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_RESET);
 HAL_SPI_TransmitReceive(&hspi1, &CTRL_REG5, &ctrl_val, 1, 100);
 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_SET);
 ctrl_val = ctrl_val | 0x08; //set FSCALE0
 uint8_t tx_buf[2];
 tx_buf[0] = CTRL_REG5 & 0x7F; //register address
 tx_buf[1] = ctrl_val; //data to write into it
 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_RESET);
 HAL_SPI_Transmit(&hspi1, tx_buf, 2, 100);
 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_SET);

 //initial dma call (deprecated)
 //HAL_SPI_TransmitReceive_DMA(&hspi1, xyz_addr, xyz_data, 6);
 //default value
 //clean_screen(0xFF, &hspi2);
 //draw_number(steps_count, 12, &hspi2);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 uint32_t steps_count_prev = -1;
 clean_screen(0xFFFF, &hspi2);
 draw_ready = 1;
 while (1)
 {

 /* USER CODE END WHILE */
 MX_USB_HOST_Process();

 /* USER CODE BEGIN 3 */
 //During each SPI clock cycle, full-duplex transmission of a single bit occurs.
 //1 clock cycle is 168/32MHz = 5.25MHz
 //meaning there are 5.25 * 10^6 bit, or 5.25 * 10^6/8 bytes = 656250 bytes
 //or, all coordinates are received 109375 times.
 if (update_lcd_flag == 1) {
 	Write_Rectangle(0, 30, 0, ILI9341_WIDTH - 1, 0xFFFF, &hspi2);
 	draw_number(steps_count, 12, &hspi2);
 	update_lcd_flag = 0;
 }
 steps_count_prev = steps_count;


 }
 /* USER CODE END 3 */
}

 SPI1 settings

cockatoo_0-1769664290410.pngcockatoo_1-1769664307679.pngcockatoo_2-1769664325610.png

Accelometer schematic

cockatoo_3-1769664359693.png

 

 

Best answer by TDK
			 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_RESET);
			 HAL_SPI_TransmitReceive_DMA(&hspi1, xyz_addr, xyz_data, 6);
			 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_SET);

DMA happens asynchronously in the background. You need to keep the CS pin low until the transaction completes.

Move the last statement to the HAL_SPI_TxRxCpltCallback callback.

 

Otherwise nothing wrong with this scheme.

1 reply

TDK
TDKBest answer
Super User
January 29, 2026
			 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_RESET);
			 HAL_SPI_TransmitReceive_DMA(&hspi1, xyz_addr, xyz_data, 6);
			 HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_SET);

DMA happens asynchronously in the background. You need to keep the CS pin low until the transaction completes.

Move the last statement to the HAL_SPI_TxRxCpltCallback callback.

 

Otherwise nothing wrong with this scheme.

"If you feel a post has answered your question, please click ""Accept as Solution""."
cockatooAuthor
Associate III
January 30, 2026

Thank you! My pedometer still doesn't work, but I guess it is for other reasons, most likely I don't use the accelerometer properly.