Skip to main content
MNapi
Senior II
August 29, 2025
Question

conflict USART and SPI

  • August 29, 2025
  • 2 replies
  • 642 views

Each time I enable SPI, it works fine.
However, whenever I include USART, SPI freezes, and this issue affects multiple chips I've tested.
SPI and USART both work well individually.


The problem seems to stem from CubeMX, which doesn't generate the code correctly.
Coding directly in Keil or CubeIDE might solve the issue, but it's time-consuming—which is exactly why we use CubeMX in the first place.


Does anyone know if this could be a simple issue, like an interrupt conflict or shared resource problem?

I looked at bunch of options like making sure the interrupt priority for USART and SPI is different.

Making sure SPI does not kick in while USART (DMA) is still processing data, ect

It's definitely a CubeMX code generation issue.
Any suggestions on how to make SPI and USART work together?

 

 

 

 

 

2 replies

Andrew Neil
Super User
August 29, 2025

@MNapi wrote:

whenever I include USART, SPI freezes


What, exactly, "freezes" ?

On what hardware?

I have used SPI and USART via CubeMX with no problem - so it must be something you're doing.

Show a minimum but complete example which illustrates the issue.

 

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MNapi
MNapiAuthor
Senior II
August 29, 2025

Here is a portion of main.c. I can't share the full code here: as soon as I try to send data over SPI3, the system freezes. However, if I only enable SPI3 without transmitting, it works fine.

The chip I'm using is the STM32F427VGT6. I've tried different SPI speeds, including 1 Mbit/s and both faster and slower rates, but nothing seems to resolve the issue. Enabling SPI3 alone does not cause the system to freeze.

The SPI3 chip select (CS) pin is configured on PE1, so it's not a basic hardware issue like a missing connection or incorrect CS pin. It seems to be something deeper.

On other hand if I write code only for SPI3, nothing else (no SPI1, no USART1), it is working fine, sending and receiving data. Disabling FMC, DMA has no effect.

Do you see what might be wrong?

 MX_GPIO_Init();
MX_DMA_Init();
MX_SPI1_Init();
MX_USART1_UART_Init();
MX_FMC_Init();
MX_SPI3_Init(); 

 

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 160;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 8;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief SPI1 Initialization Function
 * None
 * @retval None
 */
static void MX_SPI1_Init(void)
{

 /* USER CODE BEGIN SPI1_Init 0 */

 /* USER CODE END SPI1_Init 0 */

 /* USER CODE BEGIN SPI1_Init 1 */

 /* USER CODE END SPI1_Init 1 */
 /* SPI1 parameter configuration*/
 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_MASTER;
 hspi1.Init.Direction = SPI_DIRECTION_1LINE;
 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi1.Init.NSS = SPI_NSS_SOFT;
 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 10;
 if (HAL_SPI_Init(&hspi1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI1_Init 2 */

 /* USER CODE END SPI1_Init 2 */

}

/**
 * @brief SPI3 Initialization Function
 * None
 * @retval None
 */
static void MX_SPI3_Init(void)
{

 /* USER CODE BEGIN SPI3_Init 0 */

 /* USER CODE END SPI3_Init 0 */

 /* USER CODE BEGIN SPI3_Init 1 */

 /* USER CODE END SPI3_Init 1 */
 /* SPI3 parameter configuration*/
 hspi3.Instance = SPI3;
 hspi3.Init.Mode = SPI_MODE_MASTER;
 hspi3.Init.Direction = SPI_DIRECTION_2LINES;
 hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi3.Init.NSS = SPI_NSS_SOFT;
 hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;
 hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi3.Init.CRCPolynomial = 10;
 if (HAL_SPI_Init(&hspi3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI3_Init 2 */

 /* USER CODE END SPI3_Init 2 */

}

/**
 * @brief USART1 Initialization Function
 * None
 * @retval None
 */
static void MX_USART1_UART_Init(void)
{

 /* USER CODE BEGIN USART1_Init 0 */

 /* USER CODE END USART1_Init 0 */

 /* USER CODE BEGIN USART1_Init 1 */

 /* USER CODE END USART1_Init 1 */
 huart1.Instance = USART1;
 huart1.Init.BaudRate = 38400;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART1_Init 2 */

 /* USER CODE END USART1_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA2_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA2_Stream2_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA2_Stream2_IRQn, 2, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream2_IRQn);
 /* DMA2_Stream7_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA2_Stream7_IRQn, 2, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream7_IRQn);

}

/* FMC initialization function */
static void MX_FMC_Init(void)
{

 /* USER CODE BEGIN FMC_Init 0 */

 /* USER CODE END FMC_Init 0 */

 FMC_NORSRAM_TimingTypeDef Timing = {0};

 /* USER CODE BEGIN FMC_Init 1 */

 /* USER CODE END FMC_Init 1 */

 /** Perform the SRAM1 memory initialization sequence
 */
 hsram1.Instance = FMC_NORSRAM_DEVICE;
 hsram1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
 /* hsram1.Init */
 hsram1.Init.NSBank = FMC_NORSRAM_BANK1;
 hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
 hsram1.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;
 hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
 hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
 hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
 hsram1.Init.WrapMode = FMC_WRAP_MODE_DISABLE;
 hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
 hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
 hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
 hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
 hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
 hsram1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
 hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
 hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE;
 /* Timing */
 Timing.AddressSetupTime = 1;
 Timing.AddressHoldTime = 15;
 Timing.DataSetupTime = 1;
 Timing.BusTurnAroundDuration = 1;
 Timing.CLKDivision = 16;
 Timing.DataLatency = 17;
 Timing.AccessMode = FMC_ACCESS_MODE_A;
 /* ExtTiming */

 if (HAL_SRAM_Init(&hsram1, &Timing, NULL) != HAL_OK)
 {
 Error_Handler( );
 }

 /* USER CODE BEGIN FMC_Init 2 */

 /* USER CODE END FMC_Init 2 */
}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOE, GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_1, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4|GPIO_PIN_11|GPIO_PIN_12, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_6|GPIO_PIN_7, GPIO_PIN_RESET);

 /*Configure GPIO pins : PE2 PE3 PE4 */
 GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /*Configure GPIO pin : PE5 */
 GPIO_InitStruct.Pin = GPIO_PIN_5;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /*Configure GPIO pin : PE6 */
 GPIO_InitStruct.Pin = GPIO_PIN_6;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /*Configure GPIO pin : PA4 */
 GPIO_InitStruct.Pin = GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : PC6 PC7 */
 GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pins : PA11 PA12 */
 GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : PE1 */
 GPIO_InitStruct.Pin = GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

TDK
Super User
August 31, 2025

None of this code transmits with the SPI.

> The problem seems to stem from CubeMX, which doesn't generate the code correctly.

It's definitely a CubeMX code generation issue.

Based on what?

Probably just a code bug. Keep looking.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
September 17, 2025

Moved from new thread what is the address on register A16.


Did you fix your conflict USART and SPI issue?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MNapi
MNapiAuthor
Senior II
September 17, 2025

when I disabled DMA it worked. But the loop takes longer now. Small cheap small RAM, it does not seem to handle big chunks of data well.

Andrew Neil
Super User
September 17, 2025

Please update that thread.

Moved to the relevant thread.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.