Skip to main content
Associate II
June 9, 2025
Question

Disabling usbpd on reference design

  • June 9, 2025
  • 2 replies
  • 363 views

I have a u5 dev board running a usbx msc reference design , which works fine. I'm trying to disable the usbpd side of things within the reference example. I've disabled the usbpd midlewear and peirphal port for the 2 pd pins aswell as disabling the adc input. 

 

The design compile fine, after removipng the bsp however the usb msc doesn't work. Is there something I'm missing? There was one post mentioning about removing threadx messageing ques, I did try tweaking some of the threadx code but couldn't get anything working 

 

Any ideas on how to fully remove the pd code as I'm just using usb+and usb- ldata pins.

2 replies

Technical Moderator
June 10, 2025

Hi @Sidewinder 

Using CubeMX, you can disable UCPD peripheral, DMA channels and ADC. Then, regenerate code.

Attached an example MSC without power delivery stack.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Associate II
June 15, 2025

Hi FBl.

 

Thanks for the attachment. I have tried it on my u5 dev board but still no usb enumeration. In my working msc design I disable dma,adc and pd in cubeide using the peripheral configuration and then compile the design. Once compiled the programme won't enumerate with windows. But did before removing the peripherals. Is there any application code I need to change? I compared my code against your attached design and they look identical.