Skip to main content
Associate II
January 29, 2026
Solved

ESP32/STM32 SPI with ST7701S: first command not sent, sequence stops

  • January 29, 2026
  • 5 replies
  • 464 views

 

Hello,

I am using an ST7701S LCD over 3-wire SPI (CS, SCK, SDA) with my STM32.

When I send the initialization commands from my ESP, I noticed the following:

  • The first command of the sequence is not sent.

  • The program seems to stop at the second stage, around the 100th command.

SPI is configured in master mode, polling (no DMA, no interrupts).

Example of the write function:

void ST7701_Write(uint8_t dc, uint8_t data) {
uint16_t value = ((dc & 0x01) << 8) | data;
HAL_GPIO_WritePin(LCD_CS_GPIO_Port, LCD_CS_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi2, (uint8_t *)&value, 1, HAL_MAX_DELAY);
HAL_GPIO_WritePin(LCD_CS_GPIO_Port, LCD_CS_Pin, GPIO_PIN_SET);
}

Questions:

  1. Could the first command being skipped be due to HAL/SPI initialization or state?

  2. What is the recommended method to ensure all commands are reliably sent over 3-wire SPI to ST7701S?

Thank you for your help.

Best answer by Saket_Om

Hello @Ameni 

Did you try adding a small delay juste after SPI initialization? 

5 replies

mƎALLEm
Technical Moderator
January 29, 2026

Hello,

In next time please use </> to share a code. Please read How to write your question to maximize your chances to find a solution

I invite you to edit your post to comply with the community rule.

Thank you for your understanding.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Technical Moderator
January 29, 2026

Hello @Ameni 

Did you check with the logic analyzer if the first command is really sent or not? 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
AmeniAuthor
Associate II
January 29, 2026

Hello @Saket_Om,

Yes, I checked with a logic analyzer.

In fact, the behavior is the following:

  • The very first SPI frame after reset is not transmitted (it does not appear on the bus).

  • The following frames are correctly transmitted up to a certain point.

  • As soon as a HAL_Delay() is executed in the sequence, no more frames are sent after that (the SPI bus remains completely inactive).

This behavior is exactly the same whether the LCD is connected or not, which suggests that the issue is not related to the ST7701S driver itself but rather to the STM32/HAL/ThreadX layer.

On the attached logic analyzer capture, we can see:

  • the missing first frame,

  • then valid SPI frames,

  • then no activity at all after the HAL_Delay().spi.png

Technical Moderator
January 29, 2026

Hello @Ameni 

Could you please share your code?

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
AmeniAuthor
Associate II
January 29, 2026

 

Hello ,

Sure, I will share a minimal test code and the logic analyzer capture.

I attached:

  • a screenshot from the logic analyzer showing the SPI frames,

  • and a reduced test code used to reproduce the issue.

This test gives the same behavior:

  • first SPI frame is missing,

  • SPI stops after HAL_Delay(),

  • and the result is identical whether the LCD is connected or no

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2023 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "app_threadx.h"
#include "main.h"
#include "jpeg_utils_conf.h"
#include "app_touchgfx.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "Components/mx66uw1g45g/mx66uw1g45g.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

CRC_HandleTypeDef hcrc;

DCACHE_HandleTypeDef hdcache1;
DCACHE_HandleTypeDef hdcache2;

DMA2D_HandleTypeDef hdma2d;

GPU2D_HandleTypeDef hgpu2d;

XSPI_HandleTypeDef hxspi1;

I2C_HandleTypeDef hi2c2;

JPEG_HandleTypeDef hjpeg;
DMA_HandleTypeDef handle_GPDMA1_Channel1;
DMA_HandleTypeDef handle_GPDMA1_Channel0;

LTDC_HandleTypeDef hltdc;

SPI_HandleTypeDef hspi2;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void SystemPower_Config(void);
static void MX_GPIO_Init(void);
static void MX_GPDMA1_Init(void);
static void MX_ICACHE_Init(void);
static void MX_DCACHE1_Init(void);
static void MX_DCACHE2_Init(void);
static void MX_CRC_Init(void);
static void MX_LTDC_Init(void);
static void MX_DMA2D_Init(void);
static void MX_GPU2D_Init(void);
static void MX_HSPI1_Init(void);
static void MX_I2C2_Init(void);
static void MX_JPEG_Init(void);
static void MX_SPI2_Init(void);
/* USER CODE BEGIN PFP */
void ST7701S_Reset(void);
void ST7701_Write9(uint8_t dc, uint8_t data);


void ST7701_config_test(void);
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the System Power */
 SystemPower_Config();

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_GPDMA1_Init();
 MX_ICACHE_Init();
 MX_DCACHE1_Init();
 MX_DCACHE2_Init();
 MX_CRC_Init();
 MX_LTDC_Init();
 MX_DMA2D_Init();
 MX_GPU2D_Init();
 MX_HSPI1_Init();
 MX_I2C2_Init();
 MX_JPEG_Init();
 MX_SPI2_Init();
 /* Call PreOsInit function */
 MX_TouchGFX_PreOSInit();
 /* USER CODE BEGIN 2 */
 ST7701S_Reset();
 HAL_Delay(200);
 ST7701_config_test();

 /* USER CODE END 2 */

 MX_ThreadX_Init();

 /* We should never get here as control is now taken by the scheduler */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 80;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_0;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief Power Configuration
 * @retval None
 */
static void SystemPower_Config(void)
{

 /*
 * Disable the internal Pull-Up in Dead Battery pins of UCPD peripheral
 */
 HAL_PWREx_DisableUCPDDeadBattery();

 /*
 * Switch to SMPS regulator instead of LDO
 */
 if (HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY) != HAL_OK)
 {
 Error_Handler();
 }
/* USER CODE BEGIN PWR */
/* USER CODE END PWR */
}

/**
 * @brief CRC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_CRC_Init(void)
{

 /* USER CODE BEGIN CRC_Init 0 */

 /* USER CODE END CRC_Init 0 */

 /* USER CODE BEGIN CRC_Init 1 */

 /* USER CODE END CRC_Init 1 */
 hcrc.Instance = CRC;
 hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
 hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
 hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
 hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
 hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
 if (HAL_CRC_Init(&hcrc) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CRC_Init 2 */

 /* USER CODE END CRC_Init 2 */

}

/**
 * @brief DCACHE1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_DCACHE1_Init(void)
{

 /* USER CODE BEGIN DCACHE1_Init 0 */

 /* USER CODE END DCACHE1_Init 0 */

 /* USER CODE BEGIN DCACHE1_Init 1 */

 /* USER CODE END DCACHE1_Init 1 */
 hdcache1.Instance = DCACHE1;
 hdcache1.Init.ReadBurstType = DCACHE_READ_BURST_INCR;
 if (HAL_DCACHE_Init(&hdcache1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DCACHE1_Init 2 */

 /* USER CODE END DCACHE1_Init 2 */

}

/**
 * @brief DCACHE2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_DCACHE2_Init(void)
{

 /* USER CODE BEGIN DCACHE2_Init 0 */

 /* USER CODE END DCACHE2_Init 0 */

 /* USER CODE BEGIN DCACHE2_Init 1 */

 /* USER CODE END DCACHE2_Init 1 */
 hdcache2.Instance = DCACHE2;
 hdcache2.Init.ReadBurstType = DCACHE_READ_BURST_INCR;
 if (HAL_DCACHE_Init(&hdcache2) != HAL_OK)
 {
 Error_Handler();
 }
 __HAL_RCC_SYSCFG_CLK_ENABLE();
 HAL_SYSCFG_DisableSRAMCached();
 /* USER CODE BEGIN DCACHE2_Init 2 */
 // Ensure that GPU2D texture cache does not hold any out-dated data from previous application
 __HAL_RCC_GPU2D_CLK_ENABLE();
 HAL_DCACHE_Invalidate(&hdcache2);
 /* USER CODE END DCACHE2_Init 2 */

}

/**
 * @brief DMA2D Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_DMA2D_Init(void)
{

 /* USER CODE BEGIN DMA2D_Init 0 */

 /* USER CODE END DMA2D_Init 0 */

 /* USER CODE BEGIN DMA2D_Init 1 */

 /* USER CODE END DMA2D_Init 1 */
 hdma2d.Instance = DMA2D;
 hdma2d.Init.Mode = DMA2D_R2M;
 hdma2d.Init.ColorMode = DMA2D_OUTPUT_RGB888;
 hdma2d.Init.OutputOffset = 0;
 hdma2d.Init.BytesSwap = DMA2D_BYTES_REGULAR;
 hdma2d.Init.LineOffsetMode = DMA2D_LOM_PIXELS;
 if (HAL_DMA2D_Init(&hdma2d) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DMA2D_Init 2 */

 /* USER CODE END DMA2D_Init 2 */

}

/**
 * @brief GPDMA1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPDMA1_Init(void)
{

 /* USER CODE BEGIN GPDMA1_Init 0 */

 /* USER CODE END GPDMA1_Init 0 */

 /* Peripheral clock enable */
 __HAL_RCC_GPDMA1_CLK_ENABLE();

 /* GPDMA1 interrupt Init */
 HAL_NVIC_SetPriority(GPDMA1_Channel0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(GPDMA1_Channel0_IRQn);
 HAL_NVIC_SetPriority(GPDMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(GPDMA1_Channel1_IRQn);

 /* USER CODE BEGIN GPDMA1_Init 1 */

 /* USER CODE END GPDMA1_Init 1 */
 /* USER CODE BEGIN GPDMA1_Init 2 */

 /* USER CODE END GPDMA1_Init 2 */

}

/**
 * @brief GPU2D Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPU2D_Init(void)
{

 /* USER CODE BEGIN GPU2D_Init 0 */

 /* USER CODE END GPU2D_Init 0 */

 /* USER CODE BEGIN GPU2D_Init 1 */

 /* USER CODE END GPU2D_Init 1 */
 hgpu2d.Instance = GPU2D;
 if (HAL_GPU2D_Init(&hgpu2d) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN GPU2D_Init 2 */

 /* USER CODE END GPU2D_Init 2 */

}

/**
 * @brief HSPI1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_HSPI1_Init(void)
{

 /* USER CODE BEGIN HSPI1_Init 0 */

 /* USER CODE END HSPI1_Init 0 */

 /* USER CODE BEGIN HSPI1_Init 1 */

 /* USER CODE END HSPI1_Init 1 */
 /* HSPI1 parameter configuration*/
 hxspi1.Instance = HSPI1;
 hxspi1.Init.FifoThresholdByte = 4;
 hxspi1.Init.MemoryMode = HAL_XSPI_SINGLE_MEM;
 hxspi1.Init.MemoryType = HAL_XSPI_MEMTYPE_MACRONIX;
 hxspi1.Init.MemorySize = HAL_XSPI_SIZE_1GB;
 hxspi1.Init.ChipSelectHighTimeCycle = 2;
 hxspi1.Init.FreeRunningClock = HAL_XSPI_FREERUNCLK_DISABLE;
 hxspi1.Init.ClockMode = HAL_XSPI_CLOCK_MODE_0;
 hxspi1.Init.WrapSize = HAL_XSPI_WRAP_NOT_SUPPORTED;
 hxspi1.Init.ClockPrescaler = 0;
 hxspi1.Init.SampleShifting = HAL_XSPI_SAMPLE_SHIFT_NONE;
 hxspi1.Init.DelayHoldQuarterCycle = HAL_XSPI_DHQC_DISABLE;
 hxspi1.Init.ChipSelectBoundary = HAL_XSPI_BONDARYOF_NONE;
 hxspi1.Init.MaxTran = 0;
 hxspi1.Init.Refresh = 0;
 if (HAL_XSPI_Init(&hxspi1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN HSPI1_Init 2 */

 // Reset flash
 MX66UW1G45G_ResetEnable(&hxspi1, MX66UW1G45G_SPI_MODE, MX66UW1G45G_STR_TRANSFER);
 MX66UW1G45G_ResetMemory(&hxspi1, MX66UW1G45G_SPI_MODE, MX66UW1G45G_STR_TRANSFER);
 HAL_Delay(MX66UW1G45G_RESET_MAX_TIME);
 
 /* Enable write operations */
 MX66UW1G45G_WriteEnable(&hxspi1, MX66UW1G45G_SPI_MODE, MX66UW1G45G_STR_TRANSFER);

 /* Write Configuration register 2 (with new dummy cycles) */
 MX66UW1G45G_WriteCfg2Register(&hxspi1, MX66UW1G45G_SPI_MODE, MX66UW1G45G_STR_TRANSFER, MX66UW1G45G_CR2_REG3_ADDR, MX66UW1G45G_CR2_DC_6_CYCLES);

 /* Enable write operations */
 MX66UW1G45G_WriteEnable(&hxspi1, MX66UW1G45G_SPI_MODE, MX66UW1G45G_STR_TRANSFER);

 /* Write Configuration register 2 (with Octal I/O SPI protocol) */
 MX66UW1G45G_WriteCfg2Register(&hxspi1, MX66UW1G45G_SPI_MODE, MX66UW1G45G_STR_TRANSFER, MX66UW1G45G_CR2_REG1_ADDR, MX66UW1G45G_CR2_DOPI);

 /* Wait that the configuration is effective and check that memory is ready */
 HAL_Delay(MX66UW1G45G_WRITE_REG_MAX_TIME);
 
 MX66UW1G45G_EnableDTRMemoryMappedMode(&hxspi1, MX66UW1G45G_OPI_MODE);
 /* USER CODE END HSPI1_Init 2 */

}

/**
 * @brief I2C2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_I2C2_Init(void)
{

 /* USER CODE BEGIN I2C2_Init 0 */

 /* USER CODE END I2C2_Init 0 */

 /* USER CODE BEGIN I2C2_Init 1 */

 /* USER CODE END I2C2_Init 1 */
 hi2c2.Instance = I2C2;
 hi2c2.Init.Timing = 0x00F07BFF;
 hi2c2.Init.OwnAddress1 = 0;
 hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c2.Init.OwnAddress2 = 0;
 hi2c2.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
 hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Analogue filter
 */
 if (HAL_I2CEx_ConfigAnalogFilter(&hi2c2, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Digital filter
 */
 if (HAL_I2CEx_ConfigDigitalFilter(&hi2c2, 0) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2C2_Init 2 */

 /* USER CODE END I2C2_Init 2 */

}

/**
 * @brief ICACHE Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ICACHE_Init(void)
{

 /* USER CODE BEGIN ICACHE_Init 0 */

 /* USER CODE END ICACHE_Init 0 */

 /* USER CODE BEGIN ICACHE_Init 1 */

 /* USER CODE END ICACHE_Init 1 */

 /** Enable instruction cache in 1-way (direct mapped cache)
 */
 if (HAL_ICACHE_ConfigAssociativityMode(ICACHE_1WAY) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_ICACHE_Enable() != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ICACHE_Init 2 */

 /* USER CODE END ICACHE_Init 2 */

}

/**
 * @brief JPEG Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_JPEG_Init(void)
{

 /* USER CODE BEGIN JPEG_Init 0 */

 /* USER CODE END JPEG_Init 0 */

 /* USER CODE BEGIN JPEG_Init 1 */

 /* USER CODE END JPEG_Init 1 */
 hjpeg.Instance = JPEG;
 if (HAL_JPEG_Init(&hjpeg) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN JPEG_Init 2 */

 /* USER CODE END JPEG_Init 2 */

}

/**
 * @brief LTDC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_LTDC_Init(void)
{

 /* USER CODE BEGIN LTDC_Init 0 */

 /* USER CODE END LTDC_Init 0 */

 LTDC_LayerCfgTypeDef pLayerCfg = {0};

 /* USER CODE BEGIN LTDC_Init 1 */

 /* USER CODE END LTDC_Init 1 */
 hltdc.Instance = LTDC;
 hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
 hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;
 hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;
 hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
 hltdc.Init.HorizontalSync = 8;
 hltdc.Init.VerticalSync = 4;
 hltdc.Init.AccumulatedHBP = 38;
 hltdc.Init.AccumulatedVBP = 26;
 hltdc.Init.AccumulatedActiveW = 518;
 hltdc.Init.AccumulatedActiveH = 506;
 hltdc.Init.TotalWidth = 548;
 hltdc.Init.TotalHeigh = 528;
 hltdc.Init.Backcolor.Blue = 0;
 hltdc.Init.Backcolor.Green = 0;
 hltdc.Init.Backcolor.Red = 0;
 if (HAL_LTDC_Init(&hltdc) != HAL_OK)
 {
 Error_Handler();
 }
 pLayerCfg.WindowX0 = 0;
 pLayerCfg.WindowX1 = 480;
 pLayerCfg.WindowY0 = 0;
 pLayerCfg.WindowY1 = 480;
 pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB565;
 pLayerCfg.Alpha = 255;
 pLayerCfg.Alpha0 = 0;
 pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;
 pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;
 pLayerCfg.FBStartAdress = 0;
 pLayerCfg.ImageWidth = 480;
 pLayerCfg.ImageHeight = 480;
 pLayerCfg.Backcolor.Blue = 0;
 pLayerCfg.Backcolor.Green = 0;
 pLayerCfg.Backcolor.Red = 0;
 if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN LTDC_Init 2 */

 /* USER CODE END LTDC_Init 2 */

}

/**
 * @brief SPI2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_SPI2_Init(void)
{

 /* USER CODE BEGIN SPI2_Init 0 */

 /* USER CODE END SPI2_Init 0 */

 SPI_AutonomousModeConfTypeDef HAL_SPI_AutonomousMode_Cfg_Struct = {0};

 /* USER CODE BEGIN SPI2_Init 1 */

 /* USER CODE END SPI2_Init 1 */
 /* SPI2 parameter configuration*/
 hspi2.Instance = SPI2;
 hspi2.Init.Mode = SPI_MODE_MASTER;
 hspi2.Init.Direction = SPI_DIRECTION_2LINES_TXONLY;
 hspi2.Init.DataSize = SPI_DATASIZE_9BIT;
 hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi2.Init.NSS = SPI_NSS_SOFT;
 hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;
 hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi2.Init.CRCPolynomial = 0x7;
 hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
 hspi2.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
 hspi2.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
 hspi2.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
 hspi2.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
 hspi2.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
 hspi2.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
 hspi2.Init.IOSwap = SPI_IO_SWAP_DISABLE;
 hspi2.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
 hspi2.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
 if (HAL_SPI_Init(&hspi2) != HAL_OK)
 {
 Error_Handler();
 }
 HAL_SPI_AutonomousMode_Cfg_Struct.TriggerState = SPI_AUTO_MODE_DISABLE;
 HAL_SPI_AutonomousMode_Cfg_Struct.TriggerSelection = SPI_GRP1_GPDMA_CH0_TCF_TRG;
 HAL_SPI_AutonomousMode_Cfg_Struct.TriggerPolarity = SPI_TRIG_POLARITY_RISING;
 if (HAL_SPIEx_SetConfigAutonomousMode(&hspi2, &HAL_SPI_AutonomousMode_Cfg_Struct) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI2_Init 2 */

 /* USER CODE END SPI2_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */
 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOI_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOE, LCD_DISP_EN_Pin|LCD_BL_CTRL_Pin, GPIO_PIN_SET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, VSYNC_FREQ_Pin|RENDER_TIME_Pin|FRAME_RATE_Pin|MCU_ACTIVE_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(LCD_CS_GPIO_Port, LCD_CS_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOD, USER_LD2_RED_Pin|USER_LD3_GREEN_Pin, GPIO_PIN_SET);

 /*Configure GPIO pin : LCD_DISP_EN_Pin */
 GPIO_InitStruct.Pin = LCD_DISP_EN_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LCD_DISP_EN_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : TP_IRQ_Pin */
 GPIO_InitStruct.Pin = TP_IRQ_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(TP_IRQ_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : LCD_BL_CTRL_Pin */
 GPIO_InitStruct.Pin = LCD_BL_CTRL_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LCD_BL_CTRL_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : USER_BUTTON_Pin */
 GPIO_InitStruct.Pin = USER_BUTTON_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_PULLDOWN;
 HAL_GPIO_Init(USER_BUTTON_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : VSYNC_FREQ_Pin RENDER_TIME_Pin FRAME_RATE_Pin MCU_ACTIVE_Pin */
 GPIO_InitStruct.Pin = VSYNC_FREQ_Pin|RENDER_TIME_Pin|FRAME_RATE_Pin|MCU_ACTIVE_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pin : LCD_CS_Pin */
 GPIO_InitStruct.Pin = LCD_CS_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LCD_CS_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : USER_LD2_RED_Pin USER_LD3_GREEN_Pin */
 GPIO_InitStruct.Pin = USER_LD2_RED_Pin|USER_LD3_GREEN_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI5_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI5_IRQn);

 /* USER CODE BEGIN MX_GPIO_Init_2 */
 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void ST7701S_Reset(void)
{

	HAL_GPIO_WritePin(LCD_DISP_EN_GPIO_Port, LCD_DISP_EN_Pin, GPIO_PIN_RESET);
	HAL_Delay(10);
	HAL_GPIO_WritePin(LCD_DISP_EN_GPIO_Port, LCD_DISP_EN_Pin, GPIO_PIN_SET);
	HAL_Delay(120);
}


void ST7701_Write(uint8_t dc, uint8_t data)
{
 uint16_t value = ((dc & 0x01) << 8) | data; // bit9 = D/C , bits[7..0] = data
 value &= 0x1FF; // garder 9 bits
 HAL_GPIO_WritePin(LCD_CS_GPIO_Port, LCD_CS_Pin, GPIO_PIN_RESET);
 HAL_SPI_Transmit(&hspi2, (uint8_t *)&value, 1, HAL_MAX_DELAY);
 HAL_GPIO_WritePin(LCD_CS_GPIO_Port, LCD_CS_Pin, GPIO_PIN_SET);
}

void ST7701_config_test(void)
{
 ST7701_Write(1, 0x55);
 ST7701_Write(1, 0x77);
 ST7701_Write(0, 0xC0);
 ST7701_Write(1, 0x3B);
 ST7701_Write(1, 0x01);
 ST7701_Write(0, 0xC2);
 ST7701_Write(1, 0x11);
 ST7701_Write(1, 0x16);
 ST7701_Write(1, 0x0E);
 ST7701_Write(0, 0x11);
 HAL_Delay(120);
 ST7701_Write(0, 0xFF);
 ST7701_Write(1, 0x77);
 ST7701_Write(1, 0x01);
 ST7701_Write(1, 0x00);
 ST7701_Write(1, 0x00);
 ST7701_Write(1, 0x13);

	}

/* USER CODE END 4 */

/**
 * @brief Period elapsed callback in non blocking mode
 * @note This function is called when TIM6 interrupt took place, inside
 * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment
 * a global variable "uwTick" used as application time base.
 * @PAram htim : TIM handle
 * @retval None
 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
 /* USER CODE BEGIN Callback 0 */

 /* USER CODE END Callback 0 */
 if (htim->Instance == TIM6)
 {
 HAL_IncTick();
 }
 /* USER CODE BEGIN Callback 1 */

 /* USER CODE END Callback 1 */
}

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

spi.png

Andrew Neil
Super User
January 29, 2026

You're not checking the return values from any of your HAL SPI calls.

Try instrumenting your code (eg, UART output) to see what's happening.

 

Have you used the debugger to see what's happening in your code?

Examples:

 


@Ameni wrote:
  • first SPI frame is missing,


Use the debugger to check if that code is ever actually executed

 


@Ameni wrote:
  • SPI stops after HAL_Delay(),


Use the debugger to see what happens after that HAL_Delay

Perhaps the HAL_Delay is hanging ... ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AmeniAuthor
Associate II
January 29, 2026

Hello,

This is actually an important point:
when I run the code under the debugger, everything works normally.

I can step over HAL_Delay(), and the execution continues correctly after it.
There is no apparent software blocking in the code flow.

However, when running without the debugger, the behavior is different:

  • first SPI frame is missing,

  • and after HAL_Delay() no more SPI activity is observed on the bus.

So the issue seems to be timing-dependent:
the presence of the debugger changes the execution speed and makes the problem disappear.

Andrew Neil
Super User
January 29, 2026

What is the role of the ESP32 in all this?

What happens if you remove it?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Super User
January 29, 2026

> after HAL_Delay() no more SPI activity is observed on the bus.

In the presented code, you have a HAL_Delay before any of the SPI activity. It would hang there if interrupts or ticks weren't working correctly or if HAL_Delay was hanging for some reason. This story just isn't adding up. Recheck your assumptions.

> What is the role of the ESP32 in all this?

+1

ESP32 is totally unrelated to STM32. What are you actually running on? Why is ESP32 mentioned?

"If you feel a post has answered your question, please click ""Accept as Solution""."