Skip to main content
Associate
July 7, 2025
Question

Ethernet Connectivity Issue

  • July 7, 2025
  • 3 replies
  • 292 views

I would like to highlight a compatibility issue we have encountered. The TL-SG116E is a smart managed switch, whereas our machine, which uses an STM32 F7 Nucleo board, is designed to operate with an unmanaged switch. As a result, we are experiencing communication errors when connecting through the TL-SG116E.
The board is getting connected or in communication when we give it a hard reset ,while the reset button is pressed. 

3 replies

Pavel A.
Super User
July 7, 2025

Ethernet issues can occur even with plain unmanaged switches, so not surprising. 

Does this problem occur with the Nucleo board, or you have a custom board?  Please try to describe "communication errors" in more details.

 

######
Senior II
July 7, 2025

Hello,

Some more things further to the above that would be useful to know regarding your setup:

  • What Phy IC are you using? 
  • What are the port negotiation settings on your switch?
  • Does your managed switch have any port lockdown settings on for example, disabling when disconnected etc.
  • When you specifically say it is designed to operate with an unmanaged switch, what features exactly are you describing?

Thanks.

Associate
July 8, 2025
  • What Phy IC are you using? 

           LAN8742A

  • What are the port negotiation settings on your switch?

          10 Mbps, 100 Mbps, 1000 Mbps  and duplex mode

  • Does your managed switch have any port lockdown settings on for example, disabling when disconnected etc.

     Not sure (Switch name-TL-SG116E)

  • When you specifically say it is designed to operate with an unmanaged switch, what features exactly are you describing?

we are using the nucleo board for ccd camera data readout and processing .