ETHERNET RMII configuration in STM32H745I-DISCO (MB1381-H745XI-B02).
Hello ST Community,
I M USING STM32H745I-DISCO (MB1381-H745XI-B02), WHICH COME DEFAULT MII MODE, TO CONFIGURE IT ON RMII, WHAT CHANGES I HAVE TO DO IN HARDWARE, IOC. AS THIS BOARD HAVE ETHERNET IC LAN8742A-CZ-TR WHICH HAVE BOTH MII,RMII PROTOCOLS.
AS I HAVE SEEN SOME VIDEOS ON ETHERNET FOR DIFFERENT STM32 CONTROLLER IN RMII, I M NOT ABLE TO GET RESULT.
I WANTED TO KNOW DO THIS BOARD CONFIGURE IN RMII, IF YES THEN TELL ME HOW I CAN DO.
HERE IS CONFIGURATION I HAVE DONE IN MY PROJECT.
| PG11 | ETH_TX_EN | ARM Cortex-M7 | n/a | Alternate Function Push Pull | No pull-up and no pull-down | Very High | n/a | true | |
| PG14 | ETH_TXD1 | ARM Cortex-M7 | n/a | Alternate Function Push Pull | No pull-up and no pull-down | Very High | n/a | true | |
| PG13 | ETH_TXD0 | ARM Cortex-M7 | n/a | Alternate Function Push Pull | No pull-up and no pull-down | Very High | n/a | true | |
| PC5 | ETH_RXD1 | ARM Cortex-M7 | n/a | Alternate Function Push Pull | No pull-up and no pull-down | Very High | n/a | true | |
| PC4 | ETH_RXD0 | ARM Cortex-M7 | n/a | Alternate Function Push Pull | No pull-up and no pull-down | Very High | n/a | true | |
| PA1 | ETH_REF_CLK | ARM Cortex-M7 | n/a | Alternate Function Push Pull | No pull-up and no pull-down | Very High | n/a | true | |
| PA2 | ETH_MDIO | ARM Cortex-M7 | n/a | Alternate Function Push Pull | No pull-up and no pull-down | Very High | n/a | true | |
| PC1 | ETH_MDC | ARM Cortex-M7 | n/a | Alternate Function Push Pull | No pull-up and no pull-down | Very High | n/a | true | |
| PA7 | ETH_CRS_DV | ARM Cortex-M7 | n/a | Alternate Function Push Pull | No pull-up and no pull-down | Very High | n/a | true |