Skip to main content
Associate II
August 6, 2025
Solved

FLASH_OB_GetUser() wrongly reports OB_USER_SWAP_BANK bit

  • August 6, 2025
  • 3 replies
  • 462 views

In stm32u5xx_hal_flash_ex.c, version 1.6.2, FLASH_OB_GetUser() is defined as:

/**
* @brief Return the FLASH User Option Byte value.
* @retval The FLASH User Option Bytes values.
* The return value can be a combination of @ref FLASH_OB_USER_BOR_LEVEL,
* @ref FLASH_OB_USER_nRST_STOP, @ref FLASH_OB_USER_nRST_STANDBY,
* @ref FLASH_OB_USER_nRST_SHUTDOWN, @ref FLASH_OB_USER_SRAM_RST,
* @ref FLASH_OB_USER_IWDG_SW, @ref FLASH_OB_USER_IWDG_STOP,
* @ref FLASH_OB_USER_IWDG_STANDBY, @ref FLASH_OB_USER_WWDG_SW,
* @ref OB_USER_SWAP_BANK, @ref FLASH_OB_USER_DUALBANK,
* @ref FLASH_OB_USER_BKPRAM_RST, @ref FLASH_OB_USER_SRAM3_ECC,
* @ref FLASH_OB_USER_SRAM2_ECC, @ref FLASH_OB_USER_SRAM2_RST,
* @ref FLASH_OB_USER_nSWBOOT0, @ref FLASH_OB_USER_nBOOT0,
* @ref FLASH_OB_USER_PA15_PUPEN, @ref FLASH_OB_USER_IO_VDD_HSLV,
* @ref FLASH_OB_USER_IO_VDDIO2_HSLV and @ref OB_USER_TZEN
*/
static uint32_t FLASH_OB_GetUser(void)
{
uint32_t user_config = READ_REG(FLASH->OPTR);
CLEAR_BIT(user_config, FLASH_OPTR_RDP);

return user_config;
}

 

The reference to OB_USER_SWAP_BANK seems significant, since all the others are prefixed with FLASH_.

This turns out to be misleading, and unpacking the intent is confusing.

OB_USER_SWAP_BANK is 0x200, which does not correspond to a relevant bit in FLASH->OPTR. Like the other return values, I think this should be the defgroup FLASH_OB_USER_SWAP_BANK instead. The options in that group include OB_SWAP_BANK_ENABLE, defined as FLASH_OPTR_SWAP_BANK, which is indeed the SWAP_BANK bit (1<<20) in FLASH->OPTR.

 

As far as I can tell, OB_USER_SWAP_BANK should only be used as a UserType in FLASH_OB_UserConfig(). Which means the comments on that function, the FLASH_OBProgramInitTypeDef struct, and the FLASH_OB_USER_Type defgroup are all back to front as well. That means all the IS_OB_USER_* defines are misleadingly named as well. Correcting these to make a distinction between the FLASH_OB_USER_* defgroups, and the OB_USER_* UserTypes seems readily achievable and a big improvement in usability.

Best answer by Saket_Om

Hello  @liteyear 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: 215482 (This is an internal tracking number and is not accessible or usable by customers).

3 replies

Saket_OmBest answer
Technical Moderator
August 7, 2025

Hello  @liteyear 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: 215482 (This is an internal tracking number and is not accessible or usable by customers).

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Hai
ST Employee
August 22, 2025

Hello  @liteyear,

Thank you for your feedback.

The reference @ref OB_USER_SWAP_BANK should be replaced by the corresponding type group @ref FLASH_OB_USER_SWAP_BANK, which includes defined items:

- OB_SWAP_BANK_DISABLE 

- OB_SWAP_BANK_ENABLE.

the following one:

Haifa_BEN_HSOUNA_0-1755868897527.png

It appears that the original Doxygen tag comment reference was a mistake (highlighted in yellow).

Haifa_BEN_HSOUNA_2-1755869386480.png

Besides, the FLASH_OB_GetUser() function returns the "user option-bytes type", which is a logical value defined independently of the OPTCR register bit definitions. This value is used to specify the desired option-byte type before configuring it (See listed defines below):

Haifa_BEN_HSOUNA_1-1755869120970.png

Please feel free to respond and confirm whether this resolves your request.

Best regards,
Haifa.

liteyearAuthor
Associate II
August 23, 2025

@Hai wrote:

Hello  @liteyear,

Thank you for your feedback.

The reference @ref OB_USER_SWAP_BANK should be replaced by the corresponding type group @ref FLASH_OB_USER_SWAP_BANK


Yes, that's the conclusion I came to.

 

Besides, the FLASH_OB_GetUser() function returns the "user option-bytes type", which is a logical value defined independently of the OPTCR register bit definitions.


I don't think so. That the incorrect assumption I made too, based on the comments. As you can see in the code I included in my post, it literally returns the register value. The definitions in the "FLASH_OB_USER_* groups happen to be the register bit values. The logical values only seem to be used for FLASH_OB_Config().

Thanks for following up.

Hai
ST Employee
August 25, 2025

When replacing @ref OB_USER_SWAP_BANK with @ref FLASH_OB_USER_SWAP_BANK, and @ref OB_USER_TZEN with @ref FLASH_OB_USER_TZEN, the references will match the function's return type, which corresponds to the current value of each option byte.

Hai
ST Employee
August 22, 2025

The same fix should be applied to OB_USER_TZEN by adding the FLASH_ prefix.

Haifa_BEN_HSOUNA_4-1755870052749.png