Skip to main content
Associate
December 9, 2025
Question

HAL_DMAMUX1_SYNC_DMAMUX1_CH0_EVT Trigger another DMAMUX channel

  • December 9, 2025
  • 1 reply
  • 528 views

Hardware Platform: STM32H750XBH6
Software: MDK + CubeMX FW_H7_V1.12.1
github: 
https://github.com/Q-DEBUG/DMAMUX.git

Background: The timers TIM12/LPTIM1/2/3 used by DMAMUX1/2 to generate synchronization/trigger signals for H7 peripherals are all 16-bit, resulting in low precision. To improve precision and facilitate jitter compensation (testing shows a deviation of approximately 0.3ms–0.5ms per second), I intend to use the internal 32-bit timer peripheral TIM2.

The entire chain is divided into two parts:
Part 1: DMAMUX1-CH0, using direct mode (without any synchronization signal), maps the TIM2_UP event to HAL_DMAMUX1_SYNC_DMAMUX1_CH0_EVT.
Part 2: DMAMUX1-CH1, using synchronization trigger mode , uses HAL_DMAMUX1_SYNC_DMAMUX1_CH0_EVT as the synchronization signal to trigger UART4_TX.

My current test involves modifying the original LPTIM2-triggered UART periodic output routine by changing HAL_DMAMUX1_SYNC_LPTIM2_OUT to HAL_DMAMUX1_SYNC_DMAMUX1_CH0_EVT. At present, I can only observe that Timer 2 is running normally, but the UART does not output signals periodically. Since events are cleared by hardware, it is difficult for me to observe whether HAL_DMAMUX1_SYNC_DMAMUX1_CH0_EVT is effectively generated for further troubleshooting. Therefore, I am seeking assistance.

After reviewing the manual, the register status and event generation timing diagram appear to be the same.

pic1.jpg

Key code is as follows:

uint8_t UART_BUF1[]="1:hello world\r\n";
uint8_t UART_BUF2[]="2:hello world\r\n";	
HAL_DMAEx_MultiBufferStart(&hdma_uart4_tx, UART_BUF1, &huart4.Instance->TDR, UART_BUF2,sizeof(UART_BUF1));
	ATOMIC_SET_BIT(huart4.Instance->CR3, USART_CR3_DMAT);
	HAL_LPTIM_Counter_Start(&hlptim2,37500-1);

	HAL_TIM_Base_Start(&htim2);
	HAL_TIM_PWM_Start(&htim2,TIM_CHANNEL_1);
	HAL_TIM_PWM_Start(&htim2,TIM_CHANNEL_3);

void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)
{

 HAL_DMA_MuxSyncConfigTypeDef pSyncConfig= {0};
 if(tim_baseHandle->Instance==TIM2)
 {
 /* USER CODE BEGIN TIM2_MspInit 0 */

 /* USER CODE END TIM2_MspInit 0 */
 /* TIM2 clock enable */
 __HAL_RCC_TIM2_CLK_ENABLE();

 /* TIM2 DMA Init */
 /* TIM2_UP Init */
 hdma_tim2_up.Instance = DMA1_Stream0;
 hdma_tim2_up.Init.Request = DMA_REQUEST_TIM2_UP;
 hdma_tim2_up.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_tim2_up.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_tim2_up.Init.MemInc = DMA_MINC_ENABLE;
 hdma_tim2_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
 hdma_tim2_up.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
 hdma_tim2_up.Init.Mode = DMA_NORMAL;
 hdma_tim2_up.Init.Priority = DMA_PRIORITY_LOW;
 hdma_tim2_up.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_tim2_up) != HAL_OK)
 {
 Error_Handler();
 }

 pSyncConfig.SyncSignalID = HAL_DMAMUX1_SYNC_EXTI0;
 pSyncConfig.SyncPolarity = HAL_DMAMUX_SYNC_NO_EVENT;
 pSyncConfig.SyncEnable = DISABLE;
 pSyncConfig.EventEnable = ENABLE;
 pSyncConfig.RequestNumber = 1;
 if (HAL_DMAEx_ConfigMuxSync(&hdma_tim2_up, &pSyncConfig) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_LINKDMA(tim_baseHandle,hdma[TIM_DMA_ID_UPDATE],hdma_tim2_up);

 /* USER CODE BEGIN TIM2_MspInit 1 */
//	SET_BIT(DMAMUX1_Channel0->CCR,DMAMUX_CxCR_SYNC_ID_1 | DMAMUX_CxCR_SYNC_ID_2);
//	SET_BIT(DMAMUX1_Channel0->CCR,DMAMUX_CxCR_SPOL_0);
//	SET_BIT(DMAMUX1_Channel0->CCR,DMAMUX_CxCR_SE);
//	SET_BIT(DMAMUX1_Channel0->CCR,DMAMUX_CxCR_SOIE);
		SET_BIT(DMAMUX1_Channel0->CCR,DMAMUX_CxCR_EGE);

 /* USER CODE END TIM2_MspInit 1 */
 }
}

 

1 reply

Associate
December 12, 2025

Could someone help me with this issue? Thank you very much.

Associate
December 19, 2025

I resolved the issue, and it worked as expected.

Technical Moderator
December 19, 2025

Hello @Jack_member 

Glad to hear that it worked.

Please share how you solved the issue. This information helps other community members with the same issue.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"