Skip to main content
Associate II
December 17, 2025
Question

Issue with bare metal LWIP/Wolfssl on stm32n6570-dk / can not start Handshake

  • December 17, 2025
  • 1 reply
  • 295 views

I get two errors from here:

ret = wolfSSL_connect(g_tls.ssl);

if (ret == WOLFSSL_SUCCESS) {

printf("TLS handshake OK\r\n");

g_tls.state = TLS_STATE_TLS_ESTABLISHED;

} else

{

int err = wolfSSL_get_error(g_tls.ssl, ret);

if (err == WOLFSSL_ERROR_WANT_READ ||

err == WOLFSSL_ERROR_WANT_WRITE) {

} else {

printf("TLS handshake failed: %d\r\n", err);

g_tls.state = TLS_STATE_ERROR;


ret = -1 and err = 32

No ClientHello is being sent.

This is how the main looks:

/* USER CODE BEGIN Header */

/**

******************************************************************************

* @file : main.c

* @brief : Main program body

******************************************************************************

* @attention

*

* Copyright (c) 2024 STMicroelectronics.

* All rights reserved.

*

* This software is licensed under terms that can be found in the LICENSE file

* in the root directory of this software component.

* If no LICENSE file comes with this software, it is provided AS-IS.

*

******************************************************************************

*/

/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/

#include "lwip/opt.h"

#include "lwip/init.h"

#include "netif/etharp.h"

#include "lwip/netif.h"

#include "lwip/timeouts.h"

#if LWIP_DHCP

#include "lwip/dhcp.h"

#endif

#include "ethernetif.h"

#include "main.h"

#include "app_ethernet.h"

//#include "tcp_echoserver.h"

#include "tls_client.h"

 

 

/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

#if defined(__ICCARM__)

#include <LowLevelIOInterface.h>

#endif /* __ICCARM__ */

#include "tls_client.h"

/* USER CODE END Includes */

 

/* Private typedef -----------------------------------------------------------*/

#if defined(__ICCARM__)

/* New definition from EWARM V9, compatible with EWARM8 */

int iar_fputc(int ch);

#define PUTCHAR_PROTOTYPE int iar_fputc(int ch)

#elif defined(__ARMCC_VERSION)

/* ARM Compiler 6*/

#define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)

#elif defined(__GNUC__)

#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)

#endif /* __ICCARM__ */

 

/* Private define ------------------------------------------------------------*/

/* Private macro -------------------------------------------------------------*/

/* Private variables ---------------------------------------------------------*/

struct netif gnetif;

UART_HandleTypeDef UartHandle;

 

RNG_HandleTypeDef hrng;

 

/* Private function prototypes -----------------------------------------------*/

static void SystemClock_Config(void);

static void BSP_Config(void);

static void Netif_Config(void);

static void MX_USART1_UART_Init(void);

static void RISAF_Config(void);

static void MPU_Config(void);

static void MX_RNG_Init(void);

 

 

 

/**

* @brief The application entry point.

* @retval int

*/

int main(void) {

 

/* Configure the MPU */

MPU_Config();

 

/* Enable the CPU Cache */

/* Enable I-Cache---------------------------------------------------------*/

SCB_EnableICache();

 

/* Enable D-Cache---------------------------------------------------------*/

SCB_EnableDCache();

 

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

 

/* Configure the system clock */

SystemClock_Config();

 

RISAF_Config();

 

/* Initialize all configured peripherals */

MX_USART1_UART_Init();

 

/* Configure the LEDs ...*/

BSP_Config();

 

printf("TLS 1.3 Handshake \r\n");

printf("STM32N6570 board \r\n");

printf("State: Ethernet Initialization ... \r\n");

 

/* Initialize the LwIP stack */

lwip_init();

 

/* Configure the Network interface */

Netif_Config();

 

/* UDP client connect */

// tcp_echoserver_init();

TLS_GlobalInit();

 

/* Infinite loop */

 

ip_addr_t serverIp;

IP4_ADDR(&serverIp, 192,168,50,1);

// TLS_ClientStart(&serverIp, 443);

 

static int started = 0;

 

while (1)

{

ethernetif_input(&gnetif);

sys_check_timeouts();

 

 

#if LWIP_NETIF_LINK_CALLBACK

Ethernet_Link_Periodic_Handle(&gnetif);

#endif

#if LWIP_DHCP

DHCP_Periodic_Handle(&gnetif);

#endif

if (!started &&

netif_is_up(&gnetif) &&

!ip4_addr_isany_val(*netif_ip4_addr(&gnetif))) {

 

started = 1;

 

printf("IP: %s\r\n", ip4addr_ntoa(netif_ip4_addr(&gnetif)));

printf("NM: %s\r\n", ip4addr_ntoa(netif_ip4_netmask(&gnetif)));

printf("GW: %s\r\n", ip4addr_ntoa(netif_ip4_gw(&gnetif)));

 

ip_addr_t serverIp;

IP4_ADDR(&serverIp, 192,168,50,1);

 

TLS_ClientStart(&serverIp, 11111); // besser: Port auf dem dein wolfSSL server wirklich lauscht

}

 

TLS_ClientProcess();

 

 

 

}


I used this as base:

https://github.com/ABESTM/stm32n6-classic-coremw-apps/tree/main/Projects/STM32N6570-DK/Applications/LwIP/LwIP_TCP_Echo_Server


I had to make modifications to the linker script, as it was only limited to the fsbl RAM.


1 reply

3mika3Author
Associate II
December 17, 2025

The TCP Handshake works, so it is connected to the server, but like I wrote, it is not starting the TLS Handshake.