Merging STM32N6 Projects with .a Libraries Causing Build Errors in Keil
Hello,
I'm working with the STM32N6570-DK board and trying to merge two example projects provided by ST:
Project 1 (DCMIPP):
https://github.com/STMicroelectronics/STM32CubeN6/tree/main/Projects/STM32N6570-DK/Applications/DCMIPP/DCMIPP_ContinuousModeProject 2 (USB CDC):
https://github.com/STMicroelectronics/STM32CubeN6/tree/main/Projects/NUCLEO-N657X0-Q/Applications/USBX/Ux_Device_CDC_ACM
While merging, I added the following files from Project 1(DCMIPP) into the Project 2(USB CDC) project in Keil:
1 . libn6-evision-awb_keil.a
2 . libn6-evision-st-ae_keil.a
However, I’m encountering the following build issues:
- Build target 'Ux_Device_CDC_ACM'
armclang: warning: ../../../../../../Middlewares/ST/STM32_ISP_Library/evision/Lib/libn6-evision-st-ae_keil.a: 'linker' input unused [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-mfloat-abi=hard' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-mcmse' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-gdwarf-4' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-D __MICROLIB' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-I ./RTE/_Ux_Device_CDC_ACM' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-I C:/Users/Administrator/AppData/Local/Arm/Packs/ARM/CMSIS/6.1.0/CMSIS/Core/Include' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-I C:/Users/Administrator/AppData/Local/Arm/Packs/Keil/STM32N6xx_DFP/1.0.0/Drivers/CMSIS/Device/ST/STM32N6xx/Include' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-D __UVISION_VERSION=541' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-D STM32N657xx' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-D _RTE_' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-D TX_SINGLE_MODE_SECURE' [-Wunused-command-line-argument]
assembling libn6-evision-st-ae_keil.a...
armclang: warning: ../../../../../../Middlewares/ST/STM32_ISP_Library/evision/Lib/libn6-evision-awb_keil.a: 'linker' input unused [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-mfloat-abi=hard' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-mcmse' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-gdwarf-4' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-D __MICROLIB' [-Wunused-command-line-argument]
armclang: warning: argument unused during compilation: '-I ./RTE/_Ux_Device_CDC_ACM' [-Wunused-command-line-argument]
Because of this warnings build project is failed.
Could someone please guide me:
How do i add this .a files ?
Thank you in advance for your support!