Skip to main content
Associate
November 14, 2025
Solved

object detection using USB UVC camera in stm32n6570-dk

  • November 14, 2025
  • 1 reply
  • 223 views

I have STM32N6570-DK board and need to use very small sized camera ~1x1mm 30 fps with USB UVC interface for object detection applications. As the camera does not have dcmi/csi-2 interface, I am exploring how to use USB HS Host driver and UVC class driver. Questions:

1. Is it possible to get real-time inference on UVC video stream(20-30fps) as in an example ST      provides? I have tried the example and inferencing speed is very fast.

2. Are there any example codes I can refer to for USB host and vuc class driver? 

3. or should I try find the video bridging hardware converter(UVC to DCMI parallel/MIPI CSI-2)?

4. Even if I can find CSI-2 converter, firmware development will still be very challenging for CSI interface. Is it worth trying out? DCMI parallel will be much easier to implement in coding. However, small camera does not come with parallel interface. Are my assumptions correct?

Any help/guidance/clarification would be greatly appreciated!

Thank you

Best answer by FBL

Hi @Thiha2025 

For host application, you can refer to this example.

For example, the Yolov8n (256x256x3) model achieves an inference time of 35.6 ms per frame (about 28 inferences per second), and TinyYolov2 (224x224x3) achieves 31.4 ms per frame (about 32 inferences per second) under optimal conditions (Cortex-M55 at 600 MHz, NPU at 800 MHz, VDDCORE at 0.81 V). Check this wiki: AI:STM32Cube.AI model performances - stm32mcu

Here is another example firmware with trained model TinyYolov2.

Processing a USB UVC video stream will depend on the combined time for video acquisition, pre-processing, inference, and any post-processing or display steps.

1 reply

FBLBest answer
Technical Moderator
November 14, 2025

Hi @Thiha2025 

For host application, you can refer to this example.

For example, the Yolov8n (256x256x3) model achieves an inference time of 35.6 ms per frame (about 28 inferences per second), and TinyYolov2 (224x224x3) achieves 31.4 ms per frame (about 32 inferences per second) under optimal conditions (Cortex-M55 at 600 MHz, NPU at 800 MHz, VDDCORE at 0.81 V). Check this wiki: AI:STM32Cube.AI model performances - stm32mcu

Here is another example firmware with trained model TinyYolov2.

Processing a USB UVC video stream will depend on the combined time for video acquisition, pre-processing, inference, and any post-processing or display steps.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Thiha2025Author
Associate
November 19, 2025

Hi @FBL

Thanks a lot for the advice. I will try out Azure RTOS USBX example and report back. As I do not much experience with RTOS, probably gonna take a while. Thank you.