Skip to main content
SFort.1
Associate
January 6, 2025
Question

Possible bug in LL STM32 drivers (reading injected ADC)

  • January 6, 2025
  • 1 reply
  • 818 views

I have STM32F4, using ADC3 for injected conversions. Driver code is generated using the latest CubeMX. I have 4 channels in group and was using LL_ADC_INJ_ReadConversionData12(ADC3, ADC_INJECTED_RANK_1) for reading (where rank was from 1 to 4). But the values that I got back were all exactly the same and consistent with expected value on the first channel. Accessing ADC3->JDR1 to JDR4 gives correct results. If I understand LL_ADC_INJ_ReadConversionData12 correctly, then this is a bug.

 

volatile uint32_t jsqr = ADC3->JSQR;
 volatile uint32_t j1 = ADC3->JDR1;
 volatile uint32_t j2 = ADC3->JDR2;
 volatile uint32_t j3 = ADC3->JDR3;
 volatile uint32_t j4 = ADC3->JDR4;
 volatile uint16_t h1 = LL_ADC_INJ_ReadConversionData12(ADC3, ADC_INJECTED_RANK_1);
 volatile uint16_t h2 = LL_ADC_INJ_ReadConversionData12(ADC3, ADC_INJECTED_RANK_2);
 volatile uint16_t h3 = LL_ADC_INJ_ReadConversionData12(ADC3, ADC_INJECTED_RANK_3);
 volatile uint16_t h4 = LL_ADC_INJ_ReadConversionData12(ADC3, ADC_INJECTED_RANK_4);
 volatile uint16_t regular = LL_ADC_REG_ReadConversionData12(ADC3);

 

 

 

1 reply

Technical Moderator
January 9, 2025

Hello @SFort.1 

Please share your ioc file to help our team reproduce the issue.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
SFort.1
SFort.1Author
Associate
January 9, 2025

Here's my ioc file, it's not exactly the same as when I submitted the issue, but the ADCx configuration is unchanged.

 

The function in LL looks like this:

__STATIC_INLINE uint16_t LL_ADC_INJ_ReadConversionData12(const ADC_TypeDef *ADCx, uint32_t Rank)
{
 __IO uint32_t const *preg = __ADC_PTR_REG_OFFSET(ADCx->JDR1, __ADC_MASK_SHIFT(Rank, ADC_INJ_JDRX_REGOFFSET_MASK));

 return (uint16_t)(READ_BIT(*preg,
 ADC_JDR1_JDATA)
 );
}

 

gh_rcl
Associate II
June 4, 2025

Hi,

Did you get an answer regarding this bug ?

I suspect a problem with:

#define LL_ADC_INJ_RANK_x

Regards