Skip to main content
Associate
November 6, 2025
Solved

Problem with PWM + DMA on a STM32L431

  • November 6, 2025
  • 1 reply
  • 196 views

Hello, I have a problem with a STM32L431CC generating a circular PWM burst with the DMA. I am using the Timer1 to generate 4 PWM signals on the Pins PA8, PA9, PA10, PA11. The systemclock of the Timer 1 is 80 MHz. The frequency of the PWM signal should be 20kHz. I have attached the code snipped were i configured the GPIO, Timer and DMA in the software. I get no PWM signal from the GPIO pins. When I manipulate the CCRx registers of the Timer1 with the ST Link debugger, I am able to generate PWM signals with the correct frequency and duty cycle. I suspect that the Timer1 do not make a DMA request and I am not able to find the failure. The DMA do not set any interrupt flags. Also when I manipulate the DMAR register of Timer1, I can see a valid PWM signal.

Would be great when someone can support me

Thanks Patrick

patmar_0-1762442802844.png

 

 

#define TIM1_PSC_INIT 0u 
#define TIM1_ARR_INIT 3999u /* ~20 kHz at 80MHz systemclock frequency */
#define TIM1_RCR_INIT 0u

uint16_t volatile tim1_dma_buffer[] = {
 555, /* CCR1 */
 1111, /* CCR2 */
 2222, /* CCR3 */
 3333 /* CCR4 */
}; 

LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA);
 LL_GPIO_InitTypeDef gpio = {0};
 gpio.Pin = LL_GPIO_PIN_8 | LL_GPIO_PIN_9 | LL_GPIO_PIN_10 | LL_GPIO_PIN_11;
 gpio.Mode = LL_GPIO_MODE_ALTERNATE;
 gpio.Speed = LL_GPIO_SPEED_FAST;
 gpio.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 gpio.Pull = LL_GPIO_PULL_NO; 
 gpio.Alternate = LL_GPIO_AF_1;
 LL_GPIO_Init(GPIOA, &gpio);
	LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_TIM1);
 LL_TIM_SetPrescaler(TIM1, TIM1_PSC_INIT);
 LL_TIM_SetAutoReload(TIM1, TIM1_ARR_INIT);
 LL_TIM_SetRepetitionCounter(TIM1, TIM1_RCR_INIT);
 LL_TIM_SetCounterMode(TIM1, LL_TIM_COUNTERMODE_UP);
 LL_TIM_SetClockDivision(TIM1, LL_TIM_CLOCKDIVISION_DIV1);
 LL_TIM_OC_InitTypeDef oc = {0};
 oc.OCMode = LL_TIM_OCMODE_PWM1;
 oc.OCState = LL_TIM_OCSTATE_DISABLE;
 oc.OCPolarity = LL_TIM_OCPOLARITY_HIGH;
 oc.OCIdleState = LL_TIM_OCIDLESTATE_LOW;
 oc.CompareValue = 0;
 LL_TIM_OC_Init(TIM1, LL_TIM_CHANNEL_CH1, &oc);
 oc.CompareValue = 0;
 LL_TIM_OC_Init(TIM1, LL_TIM_CHANNEL_CH2, &oc);
 oc.CompareValue = 0;
 LL_TIM_OC_Init(TIM1, LL_TIM_CHANNEL_CH3, &oc);
 oc.CompareValue = 0;
 LL_TIM_OC_Init(TIM1, LL_TIM_CHANNEL_CH4, &oc);
 LL_TIM_BDTR_InitTypeDef bdtr = {0};
 bdtr.OSSRState = LL_TIM_OSSR_DISABLE;
 bdtr.OSSIState = LL_TIM_OSSI_DISABLE;
 bdtr.LockLevel = LL_TIM_LOCKLEVEL_OFF;
 bdtr.DeadTime = 0;
 bdtr.BreakState= LL_TIM_BREAK_DISABLE;
 bdtr.AutomaticOutput = LL_TIM_AUTOMATICOUTPUT_DISABLE;
 LL_TIM_BDTR_Init(TIM1, &bdtr);
 LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
 LL_DMA_DisableChannel(DMA1, LL_DMA_CHANNEL_6); 
	LL_DMA_ConfigAddresses(DMA1, LL_DMA_CHANNEL_6, (uint32_t)tim1_dma_buffer, (uint32_t)&TIM1->DMAR, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
 LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_6, LL_DMA_DIRECTION_MEMORY_TO_PERIPH); 
 LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_6, 4); 
 LL_DMA_SetMemoryIncMode (DMA1, LL_DMA_CHANNEL_6, LL_DMA_MEMORY_INCREMENT); 
 LL_DMA_SetPeriphIncMode (DMA1, LL_DMA_CHANNEL_6, LL_DMA_PERIPH_NOINCREMENT); 
 LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_6, LL_DMA_MODE_CIRCULAR);
 LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_6, LL_DMA_PRIORITY_HIGH);
 LL_DMA_SetPeriphSize (DMA1, LL_DMA_CHANNEL_6, LL_DMA_PDATAALIGN_HALFWORD); 
 LL_DMA_SetMemorySize (DMA1, LL_DMA_CHANNEL_6, LL_DMA_MDATAALIGN_HALFWORD); 
	LL_TIM_ConfigDMABurst(TIM1, LL_TIM_DMABURST_BASEADDR_CCR1, LL_TIM_DMABURST_LENGTH_4TRANSFERS);
	LL_TIM_EnableDMAReq_UPDATE(TIM1);
	LL_TIM_EnableAllOutputs(TIM1); 
 LL_TIM_CC_EnableChannel(TIM1, LL_TIM_CHANNEL_CH1 | LL_TIM_CHANNEL_CH2 |
 LL_TIM_CHANNEL_CH3 | LL_TIM_CHANNEL_CH4);
	LL_TIM_EnableARRPreload(TIM1);
	LL_TIM_OC_DisablePreload(TIM1, LL_TIM_CHANNEL_CH1);
	LL_TIM_OC_DisablePreload(TIM1, LL_TIM_CHANNEL_CH2);
	LL_TIM_OC_DisablePreload(TIM1, LL_TIM_CHANNEL_CH3);
	LL_TIM_OC_DisablePreload(TIM1, LL_TIM_CHANNEL_CH4);
	LL_DMA_EnableIT_TC(DMA1, LL_DMA_CHANNEL_6);
	LL_DMA_EnableIT_TE(DMA1, LL_DMA_CHANNEL_6);
 LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_6); 
	LL_TIM_EnableCounter(TIM1); 

 

 

Best answer by waclawek.jan

Debug as usually: read out and check/post TIM and DMA registers content. 

Where do you set the DMA request selector? I don't understand the Cube/LL gobbledygook.

JW

1 reply

waclawek.jan
waclawek.janBest answer
Super User
November 6, 2025

Debug as usually: read out and check/post TIM and DMA registers content. 

Where do you set the DMA request selector? I don't understand the Cube/LL gobbledygook.

JW

patmarAuthor
Associate
November 6, 2025

Thanks a lot for the hint with the DMA request selector. This was missing