Problem with TrustZone in STM32L562E-DK: template TrustZoneEnabled does not pass to the no-secure world
Hello everyone,
I'm working with an STM32L562E-DK board and testing the "TrustZoneEnabled" template included in the "STM32Cube_FW_L5_V1.6.0" package. The goal is to run the basic example that transitions from the secure to the unsecured zone, but I'm finding that, after following all the instructions in "README.txt" and compiling the project, the code gets stuck in the next function:
static void NonSecure_Init(void)
{
funcptr_NS NonSecure_ResetHandler;
SCB_NS->VTOR = VTOR_TABLE_NS_START_ADDR;
/* Set non-secure main stack (MSP_NS) */
__TZ_set_MSP_NS((*(uint32_t *)VTOR_TABLE_NS_START_ADDR));
/* Get non-secure reset handler */
NonSecure_ResetHandler = (funcptr_NS)(*((uint32_t *)((VTOR_TABLE_NS_START_ADDR) + 4U)));
/* Start non-secure state software application */
NonSecure_ResetHandler();
}Specifically on the "NonSecure_ResetHandler()"; or it doesn't even execute the no-secure part.
Current option bytes configuration (verified with STM32CubeProgrammer):
- DBANK => Checked
- TZEN => Checked
- nSWBOOT0 => Checked
- nBOOT0=> Unchecked
NSBOOTADD0 => Value: 0x100000 => Address: 0x08000000
NSBOOTADD1 => Value: 0x17f200 => Address: 0x0bf90000
- SECBOOTADD0 => Value: 0x1 => Address: 0x00000080
- SECWM1_PSTRT => Value: 0x0 => Address: 0x08000000
- SECWM1_PEND => Value: 0x7F => Address: 0x0803f800
- SECWM2_PSTRT => Value: 0x1 => Address: 0x08040800
- SECWM2_PEND => Value: 0x0 => Address: 0x08040000