Skip to main content
Associate III
August 9, 2025
Solved

Spi CLK late return to idle state after master tx complete

  • August 9, 2025
  • 1 reply
  • 275 views

Hi,

 

I am using an STM32H523 MCU where I transmit some data via SPI (master tx only) in blocking mode.
In debug build the SPI behaves as it should be and everything is fine.

In release build the SPI CLK line remains high for too long, after the last bit of a transmission has been sent.
This results in the (software) CS line going high before the CLK returned to 0 (the DAC7562 slave does not like that)

How it looks like in Release:
WhoIsJohnGalt_1-1754746267548.png

How it looks like in Debug (correct):

WhoIsJohnGalt_0-1754746155358.png

My code for the transmits:

 HAL_GPIO_WritePin(GPIOA, CS_Pin, GPIO_PIN_RESET);
 hal_status = HAL_SPI_Transmit(spi_handle_, data, sizeof(data), HAL_MAX_DELAY);
 HAL_GPIO_WritePin(GPIOA, CS_Pin, GPIO_PIN_SET);

 

CubeMX config code:

void MX_SPI1_Init(void)
{
 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_MASTER;
 hspi1.Init.Direction = SPI_DIRECTION_2LINES_TXONLY;
 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi1.Init.NSS = SPI_NSS_SOFT;
 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 0x7;
 hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
 hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
 hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
 hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
 hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
 hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
 hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
 hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
 hspi1.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
 hspi1.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
 if (HAL_SPI_Init(&hspi1) != HAL_OK)
 {
 Error_Handler();
 }
}
void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)
{

 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(spiHandle->Instance==SPI1)
 {
 /* USER CODE BEGIN SPI1_MspInit 0 */

 /* USER CODE END SPI1_MspInit 0 */
 /* SPI1 clock enable */
 __HAL_RCC_SPI1_CLK_ENABLE();

 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**SPI1 GPIO Configuration
 PA5 ------> SPI1_SCK
 PA7 ------> SPI1_MOSI
 */
 GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_7;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 }
}


It's the first time I see this (also the first time I use an SPI on an H5 MCU)
Does anybody have a guess what causes this issue?

In the mean time I will try using the interrupt tx function and wait in a while loop for completion.

Thanks :)

 

Regards,
Howard

Best answer by TDK

It's probably floating which would be apparent on an analog capture.

> SPI_MASTER_KEEP_IO_STATE_DISABLE

Set this enabled if you want the pins to keep their state.

1 reply

TDK
TDKBest answer
Super User
August 9, 2025

It's probably floating which would be apparent on an analog capture.

> SPI_MASTER_KEEP_IO_STATE_DISABLE

Set this enabled if you want the pins to keep their state.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate III
August 9, 2025

Yes, thanks! Have a nice weekend