STM32 USB Camera (UVC) Evaluation Board and Controller Support ?
Hi Team,
We are planning to use an STM32 camera interface over USB using the UVC protocol in our upcoming design. We would like to understand if there are any evaluation or development boards available that can be used for initial testing.
Our key requirements are as follows:
- Image size: up to 5 MB per capture
- Capture interval: one image every 30 seconds (worst case)
- Video streaming is not required; we only need still image capture and transfer
- USB-based camera interface preferred
We would like to know:
- Whether UVC is suitable for this type of non-streaming, low-frame-rate image transfer
- If anyone has implemented a simpler or similar design successfully
- Which STM32 controller models support this use case
- Availability of any development or evaluation boards for testing the camera over USB
Please share your recommendations, reference designs, or documentation links if available.
Looking forward to your guidance.
Regards,
Sathiya