STM32C071 USB Host
I'm looking to implement USB host functionality on an STM32C071 to connect with a single device that sends/receives serial data over USB so the only class I'm interested in is CDC, but I'm having trouble using USBX (I'm not using RTOS).
For now I haven't used and read/write functions, my goal was to start by checking the functionality of the callbacks inside "app_usbx_host.c" which are: device inserted/removed/connected/disconnected, enumeration fail and no USB device found. Each one sets a different flag to be handled inside the main loop.
I put a breakpoint inside the USB IRQ and when I connect the USB device it stops execution and confirms the breakpoint has been reached, however none of my flags are ever set,.
I suspect the reason might be because I haven't done anything to link the USB peripheral to the USBX stack, if the function responsible for that is ux_host_stack_hcd_register, I have no idea how to use it. The function prototype is:
UINT _ux_host_stack_hcd_register(UCHAR *hcd_name, UINT (*hcd_init_function)(struct UX_HCD_STRUCT *), ULONG hcd_param1, ULONG hcd_param2);I'm completely lost in the description for each of the arguments.
My main.c is basically this:
#include "main.h"
#include "app_usbx_host.h"
#include <stdio.h>
#include <string.h>
UART_HandleTypeDef huart1;
HCD_HandleTypeDef hhcd_USB_DRD_FS;
uint8_t my_TX_buffer[64];
uint8_t my_RX_buffer[64];
uint16_t written_len;
// THESE ARE THE FLAGS (NOT) BEING SET INSIDE THE CALLBACKS IN "app_usbx_host.c"
extern char DEVICE_INSERTED;
extern char DEVICE_REMOVED;
extern char DEVICE_CONNECTED;
extern char DEVICE_DISCONNECTED;
extern char ENUMERATION_FAIL;
extern char NOTHING_CONNECTED;
void SystemClock_Config(void);
static void MX_USART1_UART_Init(void);
static void MX_USB_HCD_Init(void);
int main(void){
HAL_Init();
SystemClock_Config();
MX_USART1_UART_Init();
MX_USB_HCD_Init();
MX_USBX_Host_Init();
HAL_HCD_Start(&hhcd_USB_DRD_FS);
while (1){
ux_system_tasks_run();
if (DEVICE_INSERTED){
written_len = snprintf((char *) my_TX_buffer, sizeof(my_TX_buffer), "USB Device Inserted\r\n");
HAL_UART_Transmit(&huart1, my_TX_buffer, written_len, 100);
DEVICE_INSERTED = 0;
}
// REST OMITTED, all the other flags get treated in the same way here
}
}
void SystemClock_Config(void){
// OMITTED FOR CLARITY
}
static void MX_USART1_UART_Init(void){
// OMITTED, UART IS WORKING
}
static void MX_USB_HCD_Init(void){
hhcd_USB_DRD_FS.Instance = USB_DRD_FS;
hhcd_USB_DRD_FS.Init.dev_endpoints = 8;
hhcd_USB_DRD_FS.Init.Host_channels = 8;
hhcd_USB_DRD_FS.Init.speed = USBD_FS_SPEED;
hhcd_USB_DRD_FS.Init.phy_itface = HCD_PHY_EMBEDDED;
hhcd_USB_DRD_FS.Init.Sof_enable = DISABLE;
hhcd_USB_DRD_FS.Init.low_power_enable = DISABLE;
hhcd_USB_DRD_FS.Init.vbus_sensing_enable = DISABLE;
hhcd_USB_DRD_FS.Init.bulk_doublebuffer_enable = DISABLE;
hhcd_USB_DRD_FS.Init.iso_singlebuffer_enable = DISABLE;
if (HAL_HCD_Init(&hhcd_USB_DRD_FS) != HAL_OK) Error_Handler();
}
void Error_Handler(void){
__disable_irq();
while (1){}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t *file, uint32_t line){}
#endif /* USE_FULL_ASSERT */
I don't remember making significant changes to any other file apart from creating the flags inside app_usbx_host.c.
The images below contain the CubeMX settings I used.
USB peripheral configuration
Class configuration
USBX configuration
I'd be extremely grateful if anyone could tell me what I missed.
Edited to apply proper source code formatting - please see How to insert source code for future reference.