Skip to main content
Associate II
January 7, 2026
Question

STM32F103RCT6 RTC init hangs in LL_RTC_Init() on custom board (LSE/Vbat related?)

  • January 7, 2026
  • 1 reply
  • 192 views
Hello everyone,

I’m working with an STM32F103RCT6 on a custom board, and I’m trying to use the built-in RTC using ST Low-Layer (LL) drivers.

When I enter debug mode, the application gets stuck inside LL_RTC_Init(). It neither returns SUCCESS nor ERROR — it keeps looping internally, apparently waiting for a flag that never gets set.

Here is the function from my application:

 
 
void LL_RTC_Init_Custom()
{ // TODO: RTC clock needs to be set to LSE. On the dev kit, LSE isn't available
 LL_RTC_InitTypeDef rtcInit =
 { .AsynchPrescaler = RTC_CLK_PRESCALE, .OutPutSource = LL_RTC_CALIB_OUTPUT_NONE };

 ErrorStatus status = LL_RTC_Init(RTC, &rtcInit);
 if (status != SUCCESS)
 Error_Handler();
}
 

Inside this function, it stucks here, in this while loop below.

ErrorStatus LL_RTC_ExitInitMode(RTC_TypeDef *RTCx)
{
 __IO uint32_t timeout = RTC_INITMODE_TIMEOUT;
 ErrorStatus status = SUCCESS;
 uint32_t tmp = 0U;

 /* Check the parameter */
 assert_param(IS_RTC_ALL_INSTANCE(RTCx));

 /* Disable initialization mode */
 LL_RTC_EnableWriteProtection(RTCx);

 /* Wait till RTC is in INIT state and if Time out is reached exit */
 tmp = LL_RTC_IsActiveFlag_RTOF(RTCx);
 while ((timeout != 0U) && (tmp != 1U))
 {
 if (LL_SYSTICK_IsActiveCounterFlag() == 1U)
 {
 timeout --;
 }

 tmp = LL_RTC_IsActiveFlag_RTOF(RTCx);
 if (timeout == 0U)
 {
 status = ERROR;
 }
 }
 return status;
}

While debugging, it looks like LL_RTC_Init() is waiting on a ready flag (likely related to RTC clock or synchronization), but in reality that flag never becomes set, so the code loops forever.

Some additional context:

  • Custom board, not an ST dev kit

  • Using LL drivers, not HAL

  • RTC clock is intended to be LSE, but I suspect LSE may not be running or available

  • Backup domain access and RTC clock configuration may be relevant

My questions:

  1. Is this behavior expected if LSE is not present or not oscillating?

  2. Does LL_RTC_Init() block indefinitely if the RTC clock source is invalid?

  3. If I leave the Vbat pin unconnected, can RTC still work? since the Vdd is present.

  4. If the 3.3 appears at the Vbat pin can I rule out all the power related issues?

Any guidance or debugging tips would be appreciated.
Thanks in advance.


Edited to apply source code formatting - please see How to insert source code for future reference.

1 reply

Andrew Neil
Super User
January 7, 2026

@Zaeem-Ahmed wrote:
 
  • Custom board, not an ST dev kit


So you'll need to give details of your board - schematics, etc:

How to write your question to maximize your chances to find a solution

 

PS:

Also, have you tried this on an ST board - to rule out any hardware issues?

And Using ST Examples?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.