STM32F4 TIM6 initialization
- June 11, 2024
- 5 replies
- 7164 views
Dear all,
I'm working on a project based on STM32F479 and FreeRTOS. In this project the microcontroller is connected via I2C and SPI bus to other devices, such as switch ethernet and spi-uart converter. I run the initialization of these devices before the start of the FreeRTOS scheduler. Startup procedure requires switching some GPIOs and waiting a few milliseconds as described in the devices datasheet. I've manged the waiting part of the initialization using the HAL_Delay function. This project has been generated in 2019 with STM32F4 fw package 1.24.0 and an old version of STM32CubeMX.
Recently I've created a new project for the same hardware using fw package 1.28.0 and STM32CubeMX 6.11.1. I noticed that the initialization of TIM6 in stm32f4xx_hal_timebase_tim.c has been updated and HAL_InitTick function is changed (which you can find in the attachment). Now I'm experiencing a strange behaviour. During devices initialization the program remains stuck in the HAL_Delay function. Apparently TIM6 interrupt is not running before the start of the scheduler, so the global variable uwTick is not incremented and as a result HAL_Delay waits forever. I had to move the initialization of the devices after the start of the FreeRTOS scheduler to solve the issue.
Can anyone help me figure out what I'm missing?
Best regards.
Massimo G.