Skip to main content
Visitor II
February 23, 2026
Question

STM32F4 UART DMA RX – Handling variable length packets reliably?

  • February 23, 2026
  • 2 replies
  • 258 views

I’m currently working with an STM32F4 series MCU and using UART with DMA for receiving data from an external module.

The incoming data packets are variable length and don’t always end with a fixed delimiter. Right now I’m using:

  • HAL_UART_Receive_DMA()

  • Circular DMA mode

  • IDLE line interrupt to detect end of frame

However, I’m noticing occasional frame misalignment when packets arrive back-to-back with minimal delay.

A few questions:

  1. Is using the UART IDLE interrupt still considered the most reliable method for variable-length packet detection?

  2. Would switching to LL drivers improve timing control significantly in high-throughput scenarios?

  3. Are there recommended buffering strategies to avoid data corruption when processing data inside the IRQ context?

System details:

  • MCU: STM32F4

  • Baud rate: 115200

  • No RTOS currently

  • Processing happens in main loop

Any advice or production-proven approaches would be appreciated.

Thanks!

2 replies

Associate
February 23, 2026

Hello there,
The F4's IDLE interrupt missing back-to-back packets is a known hardware limitation as my knowladge, as it requires at least one full frame of silence to trigger. To make your system solve this problem, you shouldn't rely on the IDLE interrupt to perfectly frame your packets.

Instead, set up a large DMA circular buffer (which I belive you have it). Use the IDLE, Half-Transfer (HT), and Transfer Complete (TC) interrupts only to update a software 'write pointer' (reading the DMA NDTR register directly via LL macros is much faster here than HAL as you asked). Then, in your main while loop, treat that circular buffer as a continuous raw byte stream. Feed those bytes into a software State Machine that actively looks for your packet headers, length bytes, and CRCs. This way, even if packets get glued together by the DMA, your parser will slice them apart accurately. 
Note: I work F7 and H7 and they have receiver timeout proporties and it helps to provide this problem.

TDK
Super User
February 23, 2026

Use HAL_UARTEx_ReceiveToIdle_DMA which will call the HAL_UARTEx_RxEventCallback callback on the HT, TC and IDLE flags. This is the most reliable way.

Here is an example to go from:

STM32CubeF4/Projects/STM32446E-Nucleo/Examples/UART/UART_ReceptionToIdle_CircularDMA/readme.txt at 7c6a0a09ecb81b360de396479e048907563f1d10 · STMicroelectronics/STM32CubeF4

 

"If you feel a post has answered your question, please click ""Accept as Solution""."