Skip to main content
Associate
July 31, 2025
Solved

STM32G4 DAC DMA Callbacks Not Firing (HAL_DAC_ConvCpltCallbackCh1 / HalfCplt)

  • July 31, 2025
  • 2 replies
  • 516 views

 

I'm working with an STM32G431KBUx and trying to output a waveform via DAC1 using DMA and TIM6 as trigger (TRGO). I’ve successfully configured the DAC and DMA using STM32CubeMX. 

However, the DMA callbacks HAL_DAC_ConvCpltCallbackCh1 and HAL_DAC_ConvHalfCpltCallbackCh1 never get called.

Here’s what I’ve checked so far:

  • DMA handle is linked manually:
    hdac1.DMA_Handle1 = &hdma_dac1_ch1;

  • Trigger is set to Timer 6 Trigger Out event.

  • DMA is configured in Circular Mode.

  • I'm calling HAL_DAC_Start_DMA(...) with a buffer of 2 * 64 samples (12-bit aligned).

  • Callback functions are correctly named and defined in main.c:

void HAL_DAC_ConvHalfCpltCallbackCh1(DAC_HandleTypeDef *hdac1) {
// Never called
}
void HAL_DAC_ConvCpltCallbackCh1(DAC_HandleTypeDef *hdac1) {
// Never called
}
/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define DMA_BUFFER_SIZE 64
#define SAMPLE_FREQ 10000
#define OUTPUT_MID 2048
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
DAC_HandleTypeDef hdac1;
DMA_HandleTypeDef hdma_dac1_ch1;

TIM_HandleTypeDef htim6;

/* USER CODE BEGIN PV */

//const float two_pi = 2 * M_PI;

uint32_t loop_cnt = 0;
uint32_t cb_cnt = 0;
uint32_t cb_full = 0;
uint32_t cb_half = 0;

uint16_t dma_buffer[2 * DMA_BUFFER_SIZE];

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_TIM6_Init(void);
static void MX_DAC1_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
inline void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) {
 if (htim->Instance == htim6.Instance) {
 //++cb_cnt;
 //GPIOA->ODR ^= GPIO_PIN_5;
 //HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
 }
}

void do_dac(uint16_t *buffer) {
 for (int i = 0; i < DMA_BUFFER_SIZE; ++i) {
 buffer[i] = (uint16_t)((4095.0f * i) / (DMA_BUFFER_SIZE - 1)); // Пила от 0 до 4095
 }
}

//void HAL_DAC_ConvCpltCallback(DAC_HandleTypeDef *hdac1) {
void HAL_DAC_ConvCpltCallbackCh1(DAC_HandleTypeDef *hdac1) {
 //++cb_full;
// HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
	GPIOA->ODR ^= GPIO_PIN_5;
 //do_dac(&dma_buffer[DMA_BUFFER_SIZE]);
}

//void HAL_DAC_ConvHalfCpltCallback(DAC_HandleTypeDef *hdac1) {
void HAL_DAC_ConvHalfCpltCallbackCh1(DAC_HandleTypeDef *hdac1) {
	//++cb_half;
//	HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
	GPIOA->ODR ^= GPIO_PIN_5;
	//do_dac(&dma_buffer[0]);
}


/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_TIM6_Init();
 MX_DAC1_Init();
 /* USER CODE BEGIN 2 */

 HAL_TIM_Base_Start_IT(&htim6);

 hdac1.DMA_Handle1 = &hdma_dac1_ch1;

 HAL_StatusTypeDef res;
 res = HAL_DAC_Start_DMA(&hdac1, DAC_CHANNEL_1, (uint32_t*)dma_buffer, 2 * DMA_BUFFER_SIZE, DAC_ALIGN_12B_R);
 if (res != HAL_OK) {
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET); // включи навсегда, если ошибка
 Error_Handler();
 }

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */

 //uint32_t now = 0, next_tick = 1000;

 while (1)
 {
	 //now = HAL_GetTick();
//	 now = uwTick;
//
//	 if (now >= next_tick) {
//
//		 printf("Tick %lu (loop=%lu cb=%lu half=%lu full=%lu)\n", now / 1000, loop_cnt, cb_cnt, cb_half, cb_full);
//
//		 loop_cnt = 0;
//		 next_tick = now + 1000;
//
//
//	 }
//
//	 ++loop_cnt;

//	 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
	 HAL_Delay(5000);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV4;
 RCC_OscInitStruct.PLL.PLLN = 85;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief DAC1 Initialization Function
 * None
 * @retval None
 */
static void MX_DAC1_Init(void)
{

 /* USER CODE BEGIN DAC1_Init 0 */

 /* USER CODE END DAC1_Init 0 */

 DAC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN DAC1_Init 1 */

 /* USER CODE END DAC1_Init 1 */

 /** DAC Initialization
 */
 hdac1.Instance = DAC1;
 if (HAL_DAC_Init(&hdac1) != HAL_OK)
 {
 Error_Handler();
 }

 /** DAC channel OUT1 config
 */
 sConfig.DAC_HighFrequency = DAC_HIGH_FREQUENCY_INTERFACE_MODE_DISABLE;
 sConfig.DAC_DMADoubleDataMode = DISABLE;
 sConfig.DAC_SignedFormat = DISABLE;
 sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
 sConfig.DAC_Trigger = DAC_TRIGGER_T6_TRGO;
 sConfig.DAC_Trigger2 = DAC_TRIGGER_NONE;
 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
 sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_EXTERNAL;
 sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
 if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DAC1_Init 2 */

 /* USER CODE END DAC1_Init 2 */

}

/**
 * @brief TIM6 Initialization Function
 * None
 * @retval None
 */
static void MX_TIM6_Init(void)
{

 /* USER CODE BEGIN TIM6_Init 0 */

 /* USER CODE END TIM6_Init 0 */

 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM6_Init 1 */

 /* USER CODE END TIM6_Init 1 */
 htim6.Instance = TIM6;
 htim6.Init.Prescaler = 128;
 htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim6.Init.Period = 65535;
 htim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim6) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM6_Init 2 */

 /* USER CODE END TIM6_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMAMUX1_CLK_ENABLE();
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : LED_Pin */
 GPIO_InitStruct.Pin = LED_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(LED_GPIO_Port, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Best answer by KnarfB

After reading STM32G431KB DAC DMA not working - Page 3 - STMicroelectronics Community

in the DMA setup, change Data With for the Peripheral to Word.

hth

KnarfB 

2 replies

KnarfB
Super User
July 31, 2025

You may find the raw interrupt handler in the *_it.c file which dispatches the irq to HAL. Set a breakpoint there and, if it is hit, follow the path through HAL.

 

hdac1.DMA_Handle1 = &hdma_dac1_ch1; is should not be needed. See __HAL_LINKDMA in HAL_DAC_MspInit.

How are the DMA settings? Maybe you add the .ioc.

hth

KnarfB

 

VadIzmalAuthor
Associate
July 31, 2025

VadIzmal_0-1753994744059.png

 



.ioc file is attached

KnarfB
KnarfBBest answer
Super User
July 31, 2025

After reading STM32G431KB DAC DMA not working - Page 3 - STMicroelectronics Community

in the DMA setup, change Data With for the Peripheral to Word.

hth

KnarfB 

TDK
Super User
July 31, 2025

Is the DAC working as expected? Is the NDTR register changing? Is the Timer CNT register changing? The rate of samples is pretty low. It'll take a few seconds for a half-buffer to be pushed out.

"If you feel a post has answered your question, please click ""Accept as Solution""."