Question
STM32G474: HRTIM issue when blanking source is selected as comparator output
- April 1, 2026
- 1 reply
- 176 views
An issue has been encountered with the STM32G474: when the blanking source is selected for the comparator module output, the events of the HRTIM
Hi,
The complete code files are in the attachment. As shown in the picture above, for the HRTIM module of the G474, Event 4 uses COMP1 as the input source. When the output of the comparator flips due to blanking, the outputs of TA1 or TA2 of the HRTIM event do not change due to the flip of the comparator output.
Thanks.