Associate
March 19, 2026
Question
STM32H5 - I3C access to IKS4A1
- March 19, 2026
- 2 replies
- 151 views
Hello Folks,
sorry, I am quite desperate. I try to get my I3C code working, but the read consistently fails and returns a buffer with just 255s and a temperature of 350 degrees centigrade.
The weird thing is that the checks I put in work, so it looks like the assignment of the address worked. If I run the code without the sensor shield connected, the checks halt program execution.
This is the code I put together from two I3C examples - for the H503 Nucleo, there is no example for the IKS4A1 and the code at https://wiki.st.com/stm32mcu/wiki/Getting_started_with_I3C and in the AN is incomplete: