Skip to main content
Associate
September 16, 2025
Question

STM32H743ZI2 UDP via Ethernet, jumbo frames

  • September 16, 2025
  • 1 reply
  • 669 views

Using H743 ETH example from how-to-create-a-project-for-stm32h7-with-ethernet-and-lwip-stack .

I want to use jumbo frames to avoid IP fragmentation while streaming audio via UDP. So, no jumbo frames have to be received. I only care about transmitting.

Below is my StartDefaultTask function, which is called in main(). Normal transmissions under 1500bytes MTU work fine when MAX_UDP_PAYLOAD_SIZE is adjusted.

I understand work needs to be done. I've tried changing buffer sizes and adjusting values in low_level_init(), but I'm unable to get it to work.

Currently, with ^^ at 2000bytes the debugger ends up here:

Screenshot 2025-09-16 130013.png

 

void StartDefaultTask(void *argument)
{
 /* init code for LWIP */
 MX_LWIP_Init();
 /* USER CODE BEGIN 5 */
 
 #define MAX_UDP_PAYLOAD_SIZE 2000
 uint8_t large_data[MAX_UDP_PAYLOAD_SIZE];
 const char* message1 = "Hello UDP message!\n\r";

 osDelay(1000);

 ip_addr_t PC_IPADDR;
 IP_ADDR4(&PC_IPADDR, 192, 168, 1, 1);

 struct udp_pcb* my_udp = udp_new();
 udp_connect(my_udp, &PC_IPADDR, 55151);
 struct pbuf* udp_buffer = NULL;

 memset(large_data, 0xAA, MAX_UDP_PAYLOAD_SIZE);

 /* Infinite loop */
 for (;;) {
 osDelay(1000);
 /* !! PBUF_RAM is critical for correct operation !! */
 udp_buffer = pbuf_alloc(PBUF_TRANSPORT, strlen(message1), PBUF_RAM);

 if (udp_buffer != NULL) {
 memcpy(udp_buffer->payload, message1, strlen(message1));
 udp_send(my_udp, udp_buffer);
 pbuf_free(udp_buffer);
 }

 udp_buffer = pbuf_alloc(PBUF_TRANSPORT, MAX_UDP_PAYLOAD_SIZE, PBUF_RAM);

 if (udp_buffer != NULL) {
 // 5. Fill the pbuf payload with the data from our source buffer
 memcpy(udp_buffer->payload, large_data, MAX_UDP_PAYLOAD_SIZE);

 // 6. Send the packet
 udp_send(my_udp, udp_buffer);

 // 7. Free the buffer
 pbuf_free(udp_buffer);
 }

 }
 /* USER CODE END 5 */
}

 

1 reply

Technical Moderator
September 22, 2025

Hello @oguh and welcome to ST Community!

Have you followed the instructions mentioned in RM433 on how to enable Jumbo Packets?

STackPointer64_0-1758547411693.png

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.