Skip to main content
RPC
Associate III
December 22, 2025
Solved

stm32h745: Flash assignment on dual core and its partitionning

  • December 22, 2025
  • 1 reply
  • 441 views

Hello everyone,

I'm writting today because I have some questions about the memory assignment of the flash on dual core devices such as stm32h745 mcu.
I'm trying to assign a direction for the boot program, imagine 20k from "0x08000000". Afterwards I wan to assign 1.5mb for the cm7 and the rest for the cm4.
As I understand, by default the flash is separated in 2 banks, first bank for the cm7 and second one for the cm4.
I wanted to know if it was possible to use the first bank and half of the second for the cm7, and the rest for the cm4.

If so, how I should proceed to achieve that? Because I managed to set the beginning of cm4 on another memory direction by setting the FLASH_BANK2_BASE define, but I don't feel like this is the best approach.

Any ideas would be greatly appreciated.

Best regards,
RPC

 

 

Best answer by mƎALLEm

Hello,


@RPC wrote:

Hello mƎALLEm,

First of all, thanks for answering so fast.

I tried to perform that using the linker, setting directions on the FLASH.ld files of each program, but it only sets correctly the direction if programmed through stm32cubeide. 


Sorry I didn't understand that statement and what do you mean by "direction"?

 


@RPC wrote:

About the vector table, do you have any links which provides more information about its configuration and examples?


You find the vector table configuration in system_stm32h7xx.c file and the configuration is here:

#ifdef CORE_CM4

 /* Configure the Vector Table location add offset address ------------------*/
#ifdef VECT_TAB_SRAM
 SCB->VTOR = D2_AXISRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#else
 SCB->VTOR = FLASH_BANK2_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif 

#else
#ifdef CORE_CM7

 /* Configure the Vector Table location add offset address ------------------*/
#ifdef VECT_TAB_SRAM
 SCB->VTOR = D1_AXISRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#else
 SCB->VTOR = FLASH_BANK1_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif 

#else
#error Please #define CORE_CM4 or CORE_CM7
#endif 

You need to set the SCB->VTOR for each core:

CM7: SCB->VTOR = 0x8005000

CM4: SCB->VTOR = 0x8000000

1 reply

mƎALLEm
Technical Moderator
December 22, 2025

Hello,

Both cores have access to both Flash banks with no restriction.

So you need to handle that for each core:

1- In the linker file

2- Set the correct vector table (new Flash memory addresses)

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
RPC
RPCAuthor
Associate III
December 22, 2025

Hello mƎALLEm,

First of all, thanks for answering so fast.

I tried to set directions on the FLASH.ld files of each program, but it only sets correctly the direction if programmed through stm32cubeide. 
About the vector table, do you have any links which provides more information about its configuration and examples?

Thanks in advance.

 

mƎALLEm
mƎALLEmBest answer
Technical Moderator
December 22, 2025

Hello,


@RPC wrote:

Hello mƎALLEm,

First of all, thanks for answering so fast.

I tried to perform that using the linker, setting directions on the FLASH.ld files of each program, but it only sets correctly the direction if programmed through stm32cubeide. 


Sorry I didn't understand that statement and what do you mean by "direction"?

 


@RPC wrote:

About the vector table, do you have any links which provides more information about its configuration and examples?


You find the vector table configuration in system_stm32h7xx.c file and the configuration is here:

#ifdef CORE_CM4

 /* Configure the Vector Table location add offset address ------------------*/
#ifdef VECT_TAB_SRAM
 SCB->VTOR = D2_AXISRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#else
 SCB->VTOR = FLASH_BANK2_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif 

#else
#ifdef CORE_CM7

 /* Configure the Vector Table location add offset address ------------------*/
#ifdef VECT_TAB_SRAM
 SCB->VTOR = D1_AXISRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#else
 SCB->VTOR = FLASH_BANK1_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
#endif 

#else
#error Please #define CORE_CM4 or CORE_CM7
#endif 

You need to set the SCB->VTOR for each core:

CM7: SCB->VTOR = 0x8005000

CM4: SCB->VTOR = 0x8000000

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."