Skip to main content
Associate III
February 5, 2026
Question

STM32H747 (M7) – TIM3 CH4 PWM with DMA produces discontinuous/glitchy waveform for addressable LEDs

  • February 5, 2026
  • 3 replies
  • 279 views

hello everybody

 

I am programming 10 addressable Leds with PWM with DMA using the M7 cortex of an STM32H747 in a custom board.
Characteristics:

  • Clocks: SysClk 480 MHz, TIM kernel clock 240 MHz
  • Timer: TIM3, Channel 4, internal clock
  • PWM base frequency: ~770 kHz (period ≈ 1.3 µs).
  • ARR: 312‑1 (312 ticks → 240 MHz/312 ≈ 769.23 kHz).
  • DMA: Peripheral = TIM3_CCR4, Memory in RAM_D2, half‑word alignment (16‑bit duty), MemInc enabled, PeriphInc disabled, Mode = Normal.

What works

If I run the timer alone (fixed duty), the PWM is correct and stable.

The problem

When I enable PWM + DMA, the waveform becomes random/discontinuous. On the oscilloscope I see “splits” and gaps; the PWM is not continuous. For example, the first 8 bits might be high and the following 16 low (intended to represent RED), but the stream breaks unpredictably. The data buffer looks correct when inspected in the debugger.

The configuration

massimoperdigo_1-1770313239202.jpeg

massimoperdigo_0-1770313226371.png
I am using channel 4 timer 3. with internal clock source.
and DMA is configured as:

massimoperdigo_2-1770313264550.png

where data width is half word since the pulse of the PWM generator channel 4 is 16 bit value.

Here is my code. All IRQs are activated.

#define NUMTOTALLEDS 10
#define NUMCOLORS 24 //< 8 BYTESxCOLOUR
#define STARTSAFEBUFFER 50 
#define ENDSAFEBUFFER 50 
 
// Placed in RAM_D2
uint16_t pwmData[NUMCOLORS*NUMTOTALLEDS+STARTSAFEBUFFER+ENDSAFEBUFFER];

const 
uint16_t ALLRED [340] = {
// Start safe buffer
PWM_RESET, PWM_RESET, PWM_RESET ...
// 8 bits high + 8 bits low + 8 bits low (Red, gren, blue)
PWM_HIGH, PWM_HIGH, PWM_HIGH, PWM_HIGH, PWM_HIGH, PWM_HIGH, PWM_HIGH, PWM_HIGH, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW, PWM_LOW,
// End safe buffer
... PWM_RESET, PWM_LOW, PWM_LOW};

// First of all i cpy a static buffer with all the information to fill 10 leds in red
memcpy(pwmData, ALLRED, sizeof(pwmData));

// Then
 if (HAL_TIM_PWM_Start_DMA(&htim3, TIM_CHANNEL_4 , (uint32_t *)pwmData, sizeof(pwmData)) == HAL_OK) {
// It returns Ok always
}

// Callback
void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)
{
 HAL_TIM_PWM_Stop_DMA(&htim3, TIM_CHANNEL_4);
}

Everything is normal to me, but this is what my oscilloscope gets:

massimoperdigo_3-1770313742894.jpeg

with zoom (the first 8 bits are high, and the 16 folowing are low, meaning red colour (RGB)):

massimoperdigo_4-1770313840348.png

My problem is that the PWM is random, and never correct.
What can I do?
Thanks in advance,

3 replies

Visitor II
February 5, 2026

Hi,

Change in configuration in DMA for Memory from HalfWord to Byte. Do not change for Peripheral. Also change buffer pwmData and ALLRED from uint16_t to uint8_t.

Best Regards.

Associate III
February 5, 2026

Yeah,

i tried so, however i do not why (maybe is a bug) both memory an peripheral must have the same length. I mean, the GUI forces the memory size to be equal to peripheral…

 

Visitor II
February 5, 2026

Hi,

Change in the generated code, not in GUI. Only for test.

gbm
Principal
February 5, 2026

1. Why don't you use UART or SPI - much less data required.

2. I don't use HAL, so I am not an expert there but I believe the size argument for HAT_PWM_Start_DMA should be the number of items rather than size in bytes.

3. When using PWM, make sure to add one more element to the table with a value of 0, so that timer output stays at 0 between packets.

4. Make sure that pwmData is a static object, not a function's local variable.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Associate III
February 5, 2026

Thankyou.

do you know any examples using uart?

thanks ;)

gbm
Principal
February 6, 2026

Here are some code fragments for G030 - should be easy to port to any new STM32.

// initial setup - note the setting of USART CR2
	RCC->IOPENR |= RCC_IOPENR_GPIOAEN | RCC_IOPENR_GPIOBEN;
	RCC->AHBENR |= RCC_AHBENR_DMA1EN;
	RCC->APBENR2 = RCC_APBENR2_USART1EN;
	
	// the UART may also work with 8-bit frames, this requires shifting the data by one to the left (verified)
	WS_UART->BRR = (HCLK_FREQ + WSBAUD / 2) / WSBAUD;
	WS_UART->CR2 = USART_CR2_TXINV | USART_CR2_MSBFIRST | USART_CR2_DATAINV | USART_CR2_SWAP;
	WS_UART->CR3 = USART_CR3_DMAT;
	WS_UART->CR1 = USART_CR1_M1 | USART_CR1_TE | USART_CR1_UE;
	
	WS_DMACH->CPAR = (uint32_t)&WS_UART->TDR;
	
	BF2F(GPIOB->MODER, 7) = GPIO_MODER_AF;
	
	DMAMUX1_Channel0->CCR = DMAREQ_ID_USART1_TX;

	
// encoding ==============================================================
void encode(uint8_t *encbuf, const struct ledc_ *img, uint16_t nleds)
{
	// MSB-first encoding table
	static const uint8_t uenc[] = {
		0000 | 022, 0001 | 022, 0010 | 022, 0011 | 022,
		0100 | 022, 0101 | 022, 0110 | 022, 0111 | 022
	};

	for (uint16_t i = 0; i < nleds; i++)
	{
		uint32_t v = img[i].r | img[i].g << 8 | img[i].b << 16;
		for (uint8_t b = 0; b < 8; b++)
		{
			*encbuf++ = uenc[v >> 21 & 7];
			v <<= 3;
		}
	}
}

// sending ===============================================================
	encode(txbuf, ledcolor, NLEDS);
	
	WS_DMACH->CCR = 0;
	WS_DMACH->CMAR = (uint32_t)txbuf;
	WS_DMACH->CNDTR = sizeof(txbuf);
	WS_DMACH->CCR = DMA_CCR_DIR_M2P | DMA_CCR_MINC | DMA_CCR_EN;

 P9823 and similar chips will not work with 1/3 + 2/3 encoding (same for timer, SPI and UART). They require at least 4 bit slices per data bit (so 2 bits per UART frame instead of 3 used by WS2812).

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice