stm32n6 gpio interrupts: exti irqhandler missing
Dear all,
I have been modifying the VENC_SDCard_ThreadX example and wanted to start some activity based on the user button, triggered by interrupt using the usual HAL + BSP helpers to init the gpio, and registering a handler function for falling flanks.
So I tried
BSP_PB_Init(BUTTON_USER1, BUTTON_MODE_EXTI);and implemented BSP_PB_Callback().
Symptom: Hitting the button turned the program to be stuck in some unrelated irqhandler (debugger name-clash -- the defaulthandler triggered), the callback has not been triggered.
I had a look at the BSP implementationn and retried the same with HAL functions, same effect, this code in BSP_PB_Init() sparked my interest:
(void)HAL_EXTI_GetHandle(&hpb_exti[Button], BUTTON_EXTI_LINE[Button]);
(void)HAL_EXTI_RegisterCallback(&hpb_exti[Button], HAL_EXTI_COMMON_CB_ID, ButtonCallback[Button]);which registers a callback, and further down the line in stm32n6xx-hal-driver-exti.c there is an HAL_EXTI_IRQHandler implementation which is not called.
Long story short, the example code seems to miss init code for the actual EXTIxx_IRQHandler.
// GPIO C13 USER button / exti channel 13
void EXTI13_IRQHandler(void) {
HAL_EXTI_ClearPending(&hpb_exti_user, EXTI_TRIGGER_FALLING);
btnCallback(); // in my code I simply perform the action needed not going through HAL
}the IRQ handler needs a reference to the exti configuration, which the BSP code initialized:
static EXTI_HandleTypeDef hpb_exti_user;
//... near the top of main(), after calling BSP_PB_Init():
HAL_EXTI_GetHandle(&hpb_exti_user, EXTI_LINE_13); // USERI had a look at a fresh CubeMX project, and seemingly the EXTI...IRQHandler functions are not generated.
This code works, but it is a hack - did I miss some code generator option for EXTI?
Thanks for some insights
Simon