Skip to main content
Associate II
September 10, 2025
Question

STM32u5 ADC is not reading using DMA

  • September 10, 2025
  • 2 replies
  • 711 views

Split from this thread. (new question)

You might be right. However it was made based on the well described example I have found.

https://deepbluembedded.com/stm32-adc-multi-channel-scan-dma-poll-single-conversion/

I was trying tu run DMA but it was not working at all. I mean it was never transfering the data from ADC to the memory. Thats why I moved back to simpler example. Below you have DMA (one shot mode) that didn't work for me. Was trying the Circular mode as well but no change.

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef handle_GPDMA1_Channel2;

DCACHE_HandleTypeDef hdcache1;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_GPDMA1_Init(void);
static void MX_ADC1_Init(void);
static void MX_DCACHE1_Init(void);
static void MX_ICACHE_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint16_t ADC_Data[4];
int is_ADCFinished = 0;
int count = 0;

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
 /* Prevent unused argument(s) compilation warning */
 is_ADCFinished = 1;

 /* NOTE : This function should not be modified. When the callback is needed,
 function HAL_ADC_ConvCpltCallback must be implemented in the user file.
 */
}
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_GPDMA1_Init();
 MX_ADC1_Init();
 MX_DCACHE1_Init();
 MX_ICACHE_Init();
 /* USER CODE BEGIN 2 */
 HAL_ADC_Start_DMA(&hadc1, ADC_Data, 4);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 HAL_Delay(500);
	 count++;
	 HAL_ADC_Start_DMA(&hadc1, ADC_Data, 4);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 20;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 1;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC1 Initialization Function
 * None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV10;
 hadc1.Init.Resolution = ADC_RESOLUTION_14B;
 hadc1.Init.GainCompensation = 0;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 4;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_ONESHOT;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_7;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_5CYCLE;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_8;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_10;
 sConfig.Rank = ADC_REGULAR_RANK_3;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_11;
 sConfig.Rank = ADC_REGULAR_RANK_4;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief DCACHE1 Initialization Function
 * None
 * @retval None
 */
static void MX_DCACHE1_Init(void)
{

 /* USER CODE BEGIN DCACHE1_Init 0 */

 /* USER CODE END DCACHE1_Init 0 */

 /* USER CODE BEGIN DCACHE1_Init 1 */

 /* USER CODE END DCACHE1_Init 1 */
 hdcache1.Instance = DCACHE1;
 hdcache1.Init.ReadBurstType = DCACHE_READ_BURST_WRAP;
 if (HAL_DCACHE_Init(&hdcache1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DCACHE1_Init 2 */

 /* USER CODE END DCACHE1_Init 2 */

}

/**
 * @brief GPDMA1 Initialization Function
 * None
 * @retval None
 */
static void MX_GPDMA1_Init(void)
{

 /* USER CODE BEGIN GPDMA1_Init 0 */

 /* USER CODE END GPDMA1_Init 0 */

 /* Peripheral clock enable */
 __HAL_RCC_GPDMA1_CLK_ENABLE();

 /* GPDMA1 interrupt Init */
 HAL_NVIC_SetPriority(GPDMA1_Channel2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(GPDMA1_Channel2_IRQn);

 /* USER CODE BEGIN GPDMA1_Init 1 */

 /* USER CODE END GPDMA1_Init 1 */
 /* USER CODE BEGIN GPDMA1_Init 2 */

 /* USER CODE END GPDMA1_Init 2 */

}

/**
 * @brief ICACHE Initialization Function
 * None
 * @retval None
 */
static void MX_ICACHE_Init(void)
{

 /* USER CODE BEGIN ICACHE_Init 0 */

 /* USER CODE END ICACHE_Init 0 */

 /* USER CODE BEGIN ICACHE_Init 1 */

 /* USER CODE END ICACHE_Init 1 */

 /** Enable instruction cache in 1-way (direct mapped cache)
 */
 if (HAL_ICACHE_ConfigAssociativityMode(ICACHE_1WAY) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_ICACHE_Enable() != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ICACHE_Init 2 */

 /* USER CODE END ICACHE_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

2 replies

mƎALLEm
Technical Moderator
September 10, 2025
"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
aristotAuthor
Associate II
September 10, 2025

Can't get rid of the below error:

 

"make: *** No rule to make target 'C:/Users/LBzdega/Downloads/STM32CubeU5-main/Drivers/STM32U5xx_HAL_Driver/Src/stm32u5xx_hal.c', needed by 'Drivers/STM32U5xx_HAL_Driver/stm32u5xx_hal.o'. Stop."

Technical Moderator
September 11, 2025

Hello @aristot 

Could you please verify whether the file stm32u5xx_hal.c exists in the following path: "C:/Users/LBzdega/Downloads/STM32CubeU5-main/Drivers/STM32U5xx_HAL_Driver/Src"
Additionally, please check your Makefile to ensure that the path to stm32u5xx_hal.c is specified correctly.

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Saket_Om"
Visitor II
October 31, 2025

Have had adc<->dma synchronisation problems before on H7 series, fixed using the synchronous clock instead of an asynchronous PLL config. Similar symptoms, adc and dma both seem to be working correctly from a reggo perspective but seems the link between them not working. Maybe worth a try fiddling with clocks