Skip to main content
Associate
February 12, 2025
Question

STM32U545 AES GCM Tag mismatch

  • February 12, 2025
  • 3 replies
  • 1091 views

Hi,

I am trying to use the AES hardware on the STM32U545 with the STM HAL libraries.

I am able to correctly encrypt and tag an number of bytes of plain text. However, whenever I try to decrypt an encrypted message with a length not divisible by 4 I get a tag mismatch but the decrypted plain text is correct.

I am using byte size data width for everything and have no header data.

 

From what I can see is that the encryption will work for any arbitrary size, however, the decryption tag is not computed correctly, unless the size is divisible by 4. Is this expected behavior or is this an issue with the HAL?

 

Thanks!

3 replies

ST Employee
February 12, 2025

Hello @todor_digitalhealth ,

Hello as you can see in the readme file of STM32CubeU5/Projects/B-U585I-IOT02A/Examples/CRYP/CRYP_AES_GCM at main · STMicroelectronics/STM32CubeU5

"Plain text which will be authenticated and encrypted. Its size must be a multiple of 16 bytes. So if the original plain text size is not a multiple of 16 bytes, it must be padded." 
also 

  • Header that will be authenticated but not encrypted. The header size must be multiple of 16 bytes whatever the key size.
  • Initialization vector a value that is used only once within a specified context. It must be padded to 16-byte length with LSB set to 2.
  • Key is the parameter which determines the cipher text. In this example the key size is 128 bits =16 bytes but it can be tailored to 192 bits or 256 bits.

So, you need to add extra padding to your plaintext if it is not multiple of 16 to get correct tags and this is normal behavior that you are seeing.
Regards

Associate
February 13, 2025

Thanks for the quick response @STea 

I am able to successfully encrypt+tag and decrypt+verify tag if the plaintext message is 4, 8, or 12 bytes without having to pad the message. The HAL library can correctly encrypt and tag any size plaintext without any additional padding. The HAL decrypt function on the other hand can correctly decrypt the message (I get the correct plain text), however, the tag is not correct. I see that the function CRYP_AESGCM_Process in stm32u5xx_hal_cryp.c has code that handles the padding if the size is not a multiple of 16 bytes. Additionally, there is a case for setting the correct size for the tag calculation.

Thanks!

 

Associate
March 13, 2025

@STeaany thoughts on my reply above?

Associate II
May 27, 2025

I'm encountering the same problem with STM32H730.

AES-CCM:

No issues, everything works.

AES-GCM:

The HAL already handles required padding on its own.

  • Encryption and tag generation - work
  • Decryption - works
  • Tag generation after decryption - invalid.
    Tried with padded AD and/or Ciphertext as a multiple of 4 and 16 bytes; the resulting tag is always invalid.
    Without AD - the same story. But works when the ciphertext/ plaintext is multiples of 4 bytes (but not when padded to such with 0-oes at the end). I.e. ciphertext of 15 bytes won't generate a correct tag, but when it is 12 or 16 bytes, then it works

Provided more details in a new thread STM32H730 AES-GCM Tag issue - STMicroelectronics Community.