STM32U5G9: wfi() instruction does not execute, no shutdown or standby
Hello,
I have a issue with my STM32U5G9. It does not go into standby or shutdown mode. I want to achieve a wake-up by the power button of my device. The powerbutton is connected to PWR_WKUP6 (pin PB5). The button has a 100k pull-up. I verified the voltage levels with a scope (3.3V --> 0V).
I checked with the examples in the STM32CubeU5 Github repo. This my code:
void LowPower::EnterStandbyMode(void) {
PrepareForLowPower();
__disable_irq();
for(int i = WWDG_IRQn; i <= JPEG_IRQn; i++) {
NVIC_ClearPendingIRQ((IRQn_Type)i);
}
/* Enable WakeUp Pin PWR_WAKEUP_PIN6 connected to PB.5 */
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN6_LOW_0);
/* Clear all related wakeup flags*/
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG6);
HAL_DBGMCU_DisableDBGStandbyMode();
/* Enter the Standby mode */
HAL_PWR_EnterSTANDBYMode();
// If entry fails (e.g., if a debugger is attached), reset the system
NVIC_SystemReset();
}I have a similar function for shutdown mode. I tried to clear all interrupt flags to make sure the WFI() instruction executes. I have the following code in my main.c:
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the System Power */
SystemPower_Config();
/* Configure the system clock */
SystemClock_Config();
/* Configure the peripherals common clocks */
PeriphCommonClock_Config();
/* USER CODE BEGIN SysInit */
/* Uncomment to be able to debug after wake-up from Standby. Consuption will be increased */
HAL_DBGMCU_EnableDBGStandbyMode();
if (__HAL_PWR_GET_FLAG(PWR_FLAG_SBF) != RESET)
{
/* Clear Standby flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SBF);
/* Check and Clear the Wakeup flag */
if (__HAL_PWR_GET_FLAG(PWR_WAKEUP_FLAG6) != RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG6);
}
}
/* USER CODE END SysInit */I call the LowPower::EnterStandbyMode() after a long press of my power button, but it just runs into the NVIC_SystemReset(), with or without debugger connected. To test this I tried to put a while(1) loop in the main if the SBF flag is set, but it just starts normal operation.
Is there anything which can block the WFI() instruction? I use the following peripherals: LTDC, GPU2D, DMA2D, USB, I2C, SAI,TIMER, ICACHE, DCACHE, CRC, ADC, DMA, OCTOSPI, RNG. The code runs on ThreadX / TouchGFX. My assumption is standby and shutdown mode stop peripheral clocks and there is no need to disable. Is my assumption correct?
Or can ThreadX block the sleep / standby?
Thanks in advance.
Robin