Skip to main content
PM.5
Associate III
August 22, 2024
Question

STM32U5G9J- Dk board source code

  • August 22, 2024
  • 2 replies
  • 783 views

Hi,

I recently purchased a STM32U5G9J -dk board. When I power up the board, TouchGFX demo application is running.

Can you please provide the source code of this demo application.

 

2 replies

ST Employee
August 22, 2024

Hello @PM.5 

I have reported this request internally. Internal ticket number: 189199 (This is an internal tracking number and is not accessible or usable by customers).

Thank you for your contribution

MOBEJ
ST Employee
May 28, 2025

Hello @PM.5 ,

In TouchGFX Designer, we offer an example that closely resembles the demo application on the STM32U5G9J-DK board. This demo is named "TouchGFX Demo 6" and can be found within the TouchGFX Designer. This tool is available as a standalone software application, making it easy and quick to evaluate graphics and develop proof-of-concept projects. It is included in the X-Cube-TouchGFX package, which you can download from the following link: TouchGFX Designer.

Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.