Skip to main content
Associate
October 28, 2025
Solved

SysTick not firing when using FreeRTOS

  • October 28, 2025
  • 3 replies
  • 490 views

Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.

Hey Folks,

I am writing firmware on a STM32U5A5ZJ-Q board, I am using FreeRTOS, and am running into some issues with SysTick, originally noticed when HAL_Delay() would just hang. I was also able to verify that uwTick does not change (this may be strange, because SysTick->Val does change as expected). I read in some other forums that 

WARNING:
When RTOS is used, it is strongly recommended to use a HAL timebase source other than the SysTick. The HAL time base source can be changed from the Pinout tab under SYS.

 

My understanding is that an RTOS that has SysTick_Handler implemented overrides the __weak handler that exists in the generated code and thereby forces things using SysTick as their timing source to a low priority. Since I already have my code written, so can I just update my code to use a different time source? I'm not entirely sure how this works, although I did come across a STM32 FreeRTOS example that implements the following code

// located in stm32u5xx_it.c

void TIM6_IRQHandler(void) // TIM6 seems to be the go to alternative to SysTIck
{
 HAL_TIM_IRQHandler(&htim6);
}

so I am hoping it is a relatively simple switch.

Please let me know if you need more details. Any assistance would be appreciated.

-Dylan

 

 

 

Best answer by drd1202

Hi All,

I got the issue resolved. C++ was mangling my interrupt handler names so that no interrupts were firing. Originally, I had checked SysTick's counter, and that was incrementing, but the interrupt was not firing because the interrupt handler names were different under the hood. Once I updated all of my code the follow strictly C, it started working immediately. I am pretty sure there is a way to do this with C++ (I had my interrupts in extern "C" blocks to try to prevent mangling), but apparently it's somewhat tricky. Anyway, I appreciate the assistance.

3 replies

gbm
Principal
October 28, 2025

When you create your FreeRTOS project with CubeMX, it suggests to choose another timer for HAL. TIM6/7 are obvious choices.

Anyway, it's definitely a very bad idea to use any HAL_Delay() in an RTOS-based application.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
drd1202Author
Associate
October 28, 2025

Hi gbm,

Thank for the response.

I get that you should use a different timing source, but how difficult is that to work into code that is already written? My current code uses SysTick, and I want to change it to TIM6. I am assuming it's fairly doable, but I have never done embedded work before, so I am just trying to keep an eye out for gotchas.

Also, Why is it a bad idea to use HAL_Delay() in an RTOS based system? Is it just because they can cause timing issues? If so, that shouldn't be an issue, I am only using them during the system initialization and once it's up I do not use it anywhere.

gbm
Principal
October 28, 2025

To efficiently use multithreading (that's what RTOS is made for) you should relinquish control to RTOS whenever you have nothing to do. That's how osDelay() works.

HAL_Delay() spends the thread's timeslice on waiting in a loop instead of telling the RTOS to switch to some useful task for a specified waiting time. If you call HAL_Delay(5) in two threads of the same priority, each of them will wait for 10 milliseconds or more.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
drd1202Author
Associate
October 28, 2025

Hi gmb,

Understood, and I should be safe then since I don't use it after the firmware fully initializes and FreeRTOS has been started.

Back to my other question: does that sound like it might be the source of my issue? The issue is showing up before FreeRTOS? I am assuming it is relatively simple to just swap out some of my code to point to TIM6 instead.

drd1202AuthorBest answer
Associate
October 29, 2025

Hi All,

I got the issue resolved. C++ was mangling my interrupt handler names so that no interrupts were firing. Originally, I had checked SysTick's counter, and that was incrementing, but the interrupt was not firing because the interrupt handler names were different under the hood. Once I updated all of my code the follow strictly C, it started working immediately. I am pretty sure there is a way to do this with C++ (I had my interrupts in extern "C" blocks to try to prevent mangling), but apparently it's somewhat tricky. Anyway, I appreciate the assistance.