Timer synchronisation
I am using a STM32G4 MCU and STM32CubeIDE.
I want to synchronise two timers (TIM3 and TIM15) that are generating PWM signals so that they both start at the same time.
TIM3 is set to 250 kHz and the PWM is modulated via DMA on channel 1. The modulated signal is a 10 kHz sine wave.
TIM15 is set to 10 kHz and the PWM is a simple 50% duty cycle.
I need the timers to start together to ensure that the PW Modulated 10 kHz sine wave (TIM3) is synchronised to the 10 kHz PWM (TIM15).
I thought it would be straight forward enough.
I have configured TIM15 as master. In CubeMX I have set Master/Slave Mode (MSM bit) to "Enable (Trigger delayed for master/slaves simultaneous start)" and Trigger Event Selection to "Enable (CNT_EN)".
I have configured TIM3 as a slave. In CubeMX I have set Slave Mode to "Trigger Mode" and Trigger Source to "ITR6" (per the reference manual).
To the CubeIDE generated code I have added:
/* USER CODE BEGIN 2 */
HAL_TIM_PWM_Start_DMA(&htim3, TIM_CHANNEL_1, BDPos_CCRValue_Buffer, CCRValue_BufferSize);
HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_1);
/* USER CODE END 2 */BDPos_CCRValue_Buffer and CCRValue_BufferSize are a pointer to the sine wave data buffer and the buffer size.
When I run the code the timers are not synchronised. After debugging through the code I found that TIM3 starts immediately on executing HAL_TIM_PWM_Start_DMA and does not wait for TIM15 to be started. TIM15 starts when this code is executed:
/* Enable the Capture compare channel */
TIM_CCxChannelCmd(htim->Instance, Channel, TIM_CCx_ENABLE);void TIM_CCxChannelCmd(TIM_TypeDef *TIMx, uint32_t Channel, uint32_t ChannelState)
{
uint32_t tmp;
/* Check the parameters */
assert_param(IS_TIM_CC1_INSTANCE(TIMx));
assert_param(IS_TIM_CHANNELS(Channel));
tmp = TIM_CCER_CC1E << (Channel & 0x1FU); /* 0x1FU = 31 bits max shift */
/* Reset the CCxE Bit */
TIMx->CCER &= ~tmp;
/* Set or reset the CCxE Bit */
TIMx->CCER |= (uint32_t)(ChannelState << (Channel & 0x1FU)); /* 0x1FU = 31 bits max shift */
}TIM15 starts when the last line is executed (ie after /* Set or reset the CCxE Bit */).
Is there a way to make TIM3 wait for TIM15 to start?
Thanks.