Skip to main content
Associate
November 19, 2025
Question

USB_Microphone: not audio output

  • November 19, 2025
  • 3 replies
  • 265 views

Hi everyone.

I am relatively new to working with STM32 devices, and I am currently attempting to design a USB microphone with an analog input using the Nucleo-L476RG development board in combination with the X-NUCLEO-CCA02M2 USB audio expansion board. To configure the system parameters in STM32CubeIDE, I followed the procedure described at the following reference: STM32F4 USB microphone | Details | Hackaday.io.

Using this configuration, the computer successfully recognizes the device as a USB microphone; however, no audio data is being transmitted.

I have attached the relevant configuration files—usbd_audio.c, usbd_audio.h, and main.c—in case someone might help identify any mistakes or oversights in my implementation. The analog signal is acquired through a single ADC channel using DMA with interrupt callbacks. The USB audio streaming is configured for a sampling rate of 48 kHz, and Timer 8 is used to trigger the ADC conversions.

Any assistance or guidance would be greatly appreciated.


Thank you very much.

3 replies

Technical Moderator
November 20, 2025

Hi @jimmyibongo 

First, I recommend you checking X-CUBE-AUDIO-KIT.

Second, since no audio data is being transmitted, could you please provide minimum firmware to test it?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Associate
November 20, 2025

Hi @FBL 

Bellow I have attached the project.

In the meantime, I will check  X-CUBE-AUDIO-KIT.

Thanks.

Associate
November 26, 2025

Hi, everyone. 

I'm still unable to solve this.

Using the STM32L476 with the X-NUCLEO-CCA02M2 USB extension, I can detect the Mic (USB configured as a Audio Class. The problem is that I don't get audio at the output. Is there a steps to follow to perfectly configure the USB audio output? which are the function that need to be called, and from where?

I'm trying to follow this notes: Introduction to USB with STM32 - stm32mcu  Is there someone that have been able to run it? Any help and guidance will be great. 

Thanks.