1. If we are logging data for the long period (48hour or 96 hour) Sometimes garbage file create in sd card other than our create file. 2. Some times file corrupt and not open on the computer. What is the reason of this issue??
Dear Community Member, I am working on the data acquisition and logging is SD card. In this project i am using stm32l452RET6 uC to interface SD card in SDIO mode with fatfs. It is working file when we are logging for the shorter time. I am creating only two file in the sd card.
Issue 1: Some times create garbage file in the sd card other than 2 files.
Issue 2: Some times our data file corrupt and not open on the pc.
What are the reason of these issue??