Question
1. What USB mode are supported by NUCLEO-F401RE which can be used to connect with PC 2. Can board connect as USB OTG? 3. NUCLEO-F401RE driver required for PC – Windows & Linux? If yes, are they available?
- Want to Know all the USB stack supported by NUCLEO-F401RE extra of Virtual COM port, Mass storage, Debug port?
- NUCLEO-F401RE does support OTG?
- Interrupt Transfer is supported by NUCLEO-F401RE or have any near future plan to support?
- Driver for NUCLEO-F401RE is available for Linux and Windows?
- We want to configure and read Real time data from from I2C/SPI slaves and send data to PC through USB. Do you have any such sample application?