2 STM32F407 sending data to each other using DMA
I have 2 STM32F407 Discovery boards sending data back and forth to each other using usart2. Usart3 on one is just a monitor so I can see the output on a USB comm port. I'm using DMA on the receive for both and the HAL_UART_RxCpltCallback for both just sends the data back for both boards. I have to have a transmit in one of the tasks before it will work. I have a counter that advances in each callback that spins the 4 LED's so I can see if it's working because it goes too fast to spit it out to the comm port. Is there any way to slow it down? I tried putting a vTaskDelay in one of the callbacks but I don't think you can do that. I'm using STM32CubeIDE and FreeRTOS.I have attached both freertos.c files from the Core/Src/ directory. The lights spin incredibly fast and then slow down and pause once in a while.