About STM32U535CEU6 Bootloader
Hello,
I am using STM32U535CEU6 for my development.
I would like to transition to the bootloader using USB DFU with Boot0 pin kept Low, and the control performed within the application. I executed the following code right after HAL_Init();, but when I tried to connect STM32CubeProgrammer, it displayed "No DFU detected."
Where could the problem be?
After connecting via J-Link and checking the option bytes, the result was as follows:
nBOOT0: Checked (1)
nSWBOOT0: Checked (1)
NSBOOTADD1: 0x0BF90000
The code I tried is as follows:
{
void (*SysMemBootJump)(void); // Define function pointer
uint32_t BootAddr = 0x0BF90000; // Bootloader address
// Get the address of the bootloader's reset handler
SysMemBootJump = (void (*)(void)) (*((uint32_t *) (BootAddr + 4)));
// Disable interrupts
__disable_irq();
// Reset all peripherals
HAL_RCC_DeInit();
// Set the stack pointer
__set_MSP(*(uint32_t *) BootAddr);
// Jump to the bootloader
SysMemBootJump();
}
Any advice please?