Add USB connector to my stm32L452 - connections
I want to add a usb connector to my stm32L452, it is powered by an external supply (not usb). I then want to use it as a CDC device, so I can plug into my PC, and it appears as a virtual com port and/or mass storage device. I have some questions:
(1) Am I correct to connect VDDUSB to the 3.3v VDD used to supply the stm32?
(2) The only connections to the socket I was planning were USB_DP, USB_DM, & gnd. Is this correct?
(3) Do I need to do anything about the stm32 and USB detection? I have seen PA9 mentioned on the web, but this would conflict with the use of pin PA9 for an I2C bus.
(4) I was going to leave the 5v from the USB cable disconnected.