After jump to DFU Bootloader Device resets on DFU command
I use JumpToBootloader() to jump to bootloader, device enters bootloader and shows device
i then send it this command
dfu-util -d 0483:df11 -S 305737513432 -a 0 -s 0x08000000:leave -D fw.bin
and device resets
Erase [ ] 0% 0 bytesdfu-util: Error during special command "ERASE_PAGE" get_status: -9 (LIBUSB_ERROR_PIPE)
If i enter the bootloader via the BOOT pin it works fine
It is like something else needs to be reset ?
dfu-util 0.11-dev
Found DFU: [0483:df11] ver=0200, devnum=44, cfg=1, intf=0, path="20-1.2.1.2", alt=0, name="@Internal Flash /0x08000000/8*128Kg", serial="305737513432"
Found DFU: [0483:df11] ver=0200, devnum=44, cfg=1, intf=0, path="20-1.2.1.2", alt=1, name="@Option Bytes /0x5200201C/01*88 e", serial="305737513432"
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2021 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
dfu-util: Warning: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release
Opening DFU capable USB device...
Device ID 0483:df11
Device DFU version 011a
Claiming USB DFU Interface...
Setting Alternate Interface #0 ...
Determining device status...
DFU state(2) = dfuIDLE, status(0) = No error condition is present
DFU mode device DFU version 011a
Device returned transfer size 1024
DfuSe interface name: "Internal Flash "
Downloading element to address = 0x08000000, size = 135828
Erase [ ] 0% 0 bytesdfu-util: Error during special command "ERASE_PAGE" get_status: -9 (LIBUSB_ERROR_PIPE)
Return Code: 74
void JumpToBootloader(void)
{
uint32_t i=0;
void (*SysMemBootJump)(void);
/* Set the address of the entry point to bootloader */
volatile uint32_t BootAddr = 0x1FF09800;
/* Disable all interrupts */
__disable_irq();
// USB->CNTR = 0x0003;
USBD_DeInit(&hUsbDeviceHS);
HAL_DMA_DeInit(&hdma_adc3);
HAL_DMA_DeInit(&hdma_dac1_ch1);
HAL_DMA_DeInit(&hdma_dac1_ch2);
HAL_DMA_DeInit(&hdma_usart2_tx);
HAL_DMA_DeInit(&hdma_usart3_tx);
HAL_CORDIC_DeInit(&hcordic);
HAL_DAC_DeInit(&hdac1);
HAL_UART_DeInit(&huart2);
HAL_UART_DeInit(&huart3);
HAL_ADC_DeInit(&hadc3);
HAL_TIM_Base_DeInit(&htim2);
HAL_TIM_Base_DeInit(&htim3);
HAL_TIM_Base_DeInit(&htim6);
HAL_I2C_DeInit(&hi2c4);
HAL_RTC_DeInit(&hrtc);
// HAL_DeInit();
/* Disable Systick timer */
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
/* Set the clock to the default state */
HAL_RCC_DeInit();
/* Clear Interrupt Enable Register & Interrupt Pending Register */
uint8_t cnt = (sizeof(NVIC->ICER) / sizeof(NVIC->ICER[0]));
for (i=0;i<cnt;i++)
{
NVIC->ICER[i]=0xFFFFFFFF;
NVIC->ICPR[i]=0xFFFFFFFF;
}
/* Re-enable all interrupts */
__enable_irq();
/* Set up the jump to booloader address + 4 */
SysMemBootJump = (void (*)(void)) (*((uint32_t *) ((BootAddr + 4))));
/* Set the main stack pointer to the bootloader stack */
__set_MSP(*(uint32_t *)BootAddr);
/* Call the function to jump to bootloader location */
SysMemBootJump();
/* Jump is done successfully */
while (1)
{
/* Code should never reach this loop */
}
}